(1)| 9/15/2017 2:33 PM | |
|
Joined: 9/23/2005 Last visit: 12/23/2025 Posts: 5149 Rating:
|
Do you mean functions over complex numbers? Use OSCAT. Or simply look at its source to see how it can be done. |
|
Regards, |
|
| 9/15/2017 2:47 PM | |
|
Joined: 9/27/2006 Last visit: 12/24/2025 Posts: 12472 Rating:
|
Helo turkoghly: If you need documentation on the OSCAT functions in English, open the following link:
Study the "Complex" datatype, and the Complex math functions available in Chapter 7. You can download OSCAT for S7 v. 3.32 )Free of charge) here: http://www.oscat.de/component/jdownloads/summary/2-oscat-basic/8-oscat-basic-332-s7.html Hope this helps, |
| 9/15/2017 3:42 PM | |
|
Posts: 147 Rating:
|
Thank you so much for help How to add this functions to my step7 library? |
| 9/15/2017 4:03 PM | |
|
Joined: 9/27/2006 Last visit: 12/24/2025 Posts: 12472 Rating:
|
Hell turkoghly; It is a simple matter of downloading,and unzipping the OSCAT library to your Step 7 application (you will need SCL installed). Open the extraction directory to locate the family of functions you need, open the subdirectories and drag the FB/FCs you need to your Blocks directory. You may have to compile the sources. Then use them as ordinary S7 blocks. See this discussion from the OSCAT forum (very useful link, by the way for further information on OSCAT functions): http://www.oscat.de/community/index.php?topic=297.0;wap2 Hope this helps, |
| 9/15/2017 4:16 PM | |
|
Posts: 147 Rating:
|
Thank you very much |
Follow us on