×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 100744248, Entry date: 04/16/2020
(8)
Rate

Line Integration at the Food & Beverage Industry - WinCC Demo project "LineIntegration"

  • Entry
  • Associated product(s)
For the mechanical engineering industry, Siemens provides a standardized machine integration concept that enables efficient evaluation of process data for the line operator with the WinCC add-on PM-ANALYZE. The WinCC project includes modules based on the international standards of the OMAC User Group and Weihenstephan standards.

The Line HMI Library is part of the Line Integration Concept at the Food & Beverage Industry. An overview of the Line Integration Concept you can find here.


Figure 1


The "Line Integration" project contains standardized elements for the visualization of machine and line information with SIMATIC WinCC. The elements are based on the Plant Data Interface and contains the following detailed information:
  • Basic information like state and piece counter
  • Energy values for consumption and KPIs
  • KPIs for maschine and line efficiency
  • Machine specific parameters

All functions are modular and available as components for machine and line. The function blocks and the SIMATIC WinCC demo project can be easily  integrated into existing applications.

The software is based on the international standards of OMAC-User group and Weihenstephan Standards, which sets the industry-standard for the according data Interfaces.


Figure 2

Your benefits at a glance

  • Based on the standards OMAC and Weihenstephan defined by end-customers, which is worldwide existing and all-purpose
  • Minimization of the engineering time due to pre-built and tested modules.
  • Improvement of the analysis options with WinCC PM ANALYZE:
    • Transparency of plant-wide information
    • Faster decisions due to an optimal view of information with the goal of:
      • Increase availability
      • Reducing unplanned downtimes
      • Reducing failures
  • Transparent data availability for all task levels
  • Standardized plant-wide alarm structure
  • Standardized parameter interface for each machine

Validation

  • OMAC – Specification ANSI/ISA-TR88.00.02-2015 (Approved 26 October 2015)
  • Weihenstephan - Specification of the Interface Content (Version 08)
  • SIMATIC WinCC V7.5

If you have questions regarding the integration of the Demo project into your plant, contact us by e-mail using the subject: "Line Integration":
dpe-contact.de@siemens.com


Downloads
  Documentation (3,1 MB) 

WinCC LineIntegration V3 demo project
 Registrierung notwendig  WinCC V7.5 demo project (42,9 MB) 

TIA Portal V15.1 project
 Registrierung notwendig  PLC demo project (5,1 MB)

Line Integration function blocks for PM-ANALYZE
 Registrierung notwendig  LineIntegrationFunctionBlocks (194,1 KB)

Note
You will only need the file "FunctionBlocks" if you change the status model in PM-SERVER.
For editing, you need a C#-compatible editor and programming knowledge.


Last Changes 
Update the demo project to V3

Additional keywords
Line Monitoring, Machine Monitoring, Key Performance Indicator, Digitalization, Filling and Packaging, Line Performance Improvement, Standardization, Data transparency, Weihenstephan, OMAC, Linienintegration, Food and Beverage, F&B, Lebensmittelindustrie, PM-ANALYZE, OEE, Performance reporting

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.