×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 101978659, Entry date: 10/10/2014
(0)
Rate

Configuration of the model based predictive controller MPC10x10 for Tennessee Eastman Benchmark Process in SIMATIC PCS 7

  • Entry
  • Associated product(s)

Objective of the Application
In addition to the model based predictive controller ModPreCon for up to 4x4 interacting manipulated and controlled variables the new large predictive controller MPC10x10 for up to 10x10 manipulated and controlled variables is introduced in the context of PCS 7 V8.1. The MPC10x10 not only offers larger variable numbers but also some principally new functions which are introduced in this application note.
This document expands the applications notes "Model based predictive multi-variable control at the example of a distillation column" (Entry-ID 37361208) and " Fluidized bed dryer - design of a predictive controller with operating point optimization" (Entry-ID 61926069)  in which the functions of the ModPreCon are already described  and is focused on the new features of the MPC10x10.
Using the example of a processing plant with several units (Tennessee Eastman benchmark process with reactor, separator, stripper and compressor) the design of the MPC10x10 as a supervisory master controller is explained, dealing with six manipulated variables, five controlled variables and three measurable disturbance variables.

Main contents
The following issues are treated in this application:

  • Identification of  process models  with numerous manipulated and controlled variables
  • Dynamic online optimization considering  constraints
  • Setting of  target values for manipulated variables
  • Simulation studies inside  MPC configurator
  • Commissioning and test of  the controller

Validity
SIMATIC PCS 7 V8.1

Download

Content of downloads

Download

Documentation
Configuration of the MPC10x10 for Tennessee Eastman Benchmark Process
101978659_PCS7_MPC10x10_en.pdf ( 2232 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.