Entry type: FAQ, Entry ID: 1022975, Entry date: 09/04/2001
(0)
Rate

PPI connection of ProTool/Pro and S7-200

  • Entry
  • Associated product(s)

QUESTION:
Can you connect the runtime version of ProTool/Pro with an S7-200 via PPI?

ANSWER:
ProTool V5.2 / SP 1 and lower:
In the description you have read that it is possible to connect the runtime version of ProTool/Pro with an S7-200 via PPI. But a PC/PPI cable is not sufficient for this. You need the CPs CP5411, CP5511, CP5611 or MPI on-board. Also, when using the PPI protocol, you should note that only one S7-200 controller can be addressed. With MPI you can use several controllers. 

ProTool V5.2 / SP 2 and higher:
The following PC/PPI cable is released as a pure point-to-point interface between a ProTool/Pro Runtime (V5.2 / SP2 and higher) and a SIMATIC S7-200:

  • MLFB 6ES7 901-3BF20-0XA0

The necessary drivers are installed automatically with ProTool/Pro Runtime V5.2 / SP2. The drivers are released for Windows 95/98.

Keywords:
Communications

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster