×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 102379345, Entry date: 04/09/2019
(17)
Rate

SITOP PSU8600: Faceplates and Communication Blocks (TIA Portal, STEP 7 and WinCC)

  • Entry
  • Associated product(s)
Use the rapidly applicable faceplates and function blocks in this sample application to connect the controllable power supply SITOP PSU8600 to your plant. Information is also given about how to control the power supply with your PLC.

Your task is to equip your automation plant with a diagnosable and controllable power supply.
The power supply shall be communication-capable and integrated into the automation network.
It shall be possible to switch individual plant components on and off.
The status and diagnostic information of the power supply shall be displayed in the HMI stations for operator control and monitoring.

Solution
The application example shows you a possible way how to integrate the controllable power supply SITOP PSU8600 into your application network.
This introduces the diagnostic information to the controller and makes it possible for the PLC to control the power supply.

All relevant data and states of the SITOP PSU8600 are displayed conveniently on an HMI station.
For this application case, the application example provides function blocks for
SIMTAIC STEP 7 V5 and SIMATIC STEP 7 Professional (TIA Portal), as well as HMI faceplates and HMI screen windows for SIMATIC WinCC flexible 2008, SIMATIC WinCC Comfort/Advanced/Professional and SIMATIC WinCC.


Advantages

The application offers the following advantages:

  • Time and cost saving by means of provided function blocks and HMI faceplates.
  • Easy and comprehensive introduction into the topic of integrating a
    SITOP PSU8600 within a PROFINET network. 

Downloads 

  • TIA Portal
    Contents of the library: function blocks for  SIMATIC STEP 7 Professional (SIMATIC S7-300/400 and SIMATIC S7-1200/1500),
    faceplates for SIMATIC WinCC Comfort/Advanced and screen windows for SIMATIC WinCC Professional.
     

Software version
SITOP PSU8600
firmware version
 TIA Portal
(STEP 7 Professional, WinCC) 
  V1.4
V15.1  Documentation V2.4 (7,3 MB) 
 Registrierung notwendig  Library V2.4 (8,2 MB) 
 
V15  Documentation V2.4 (7,3 MB)
 Registrierung notwendig  Library V2.4 (8,4 MB)
 
V14 / V14 SP1  Documentation V2.4 (7,3 MB)
 Registrierung notwendig  Library V2.4 (9,9 MB)
 
  V1.2 V1.3
 V15---  Documentation V2.3 (6,6 MB)
 Registrierung notwendig  Library V2.3 (5,6 MB)
V14 / V14 SP1  Documentation V2.2 (6,9 MB)
 Registrierung notwendig  Library V2.2 (3,5 MB) 
  Documentation V2.3 (6,6 MB)
 Registrierung notwendig  Library V2.3 (5,8 MB) 
V13 SP1  Documentation V2.2 (6,9 MB)
 Registrierung notwendig  Library V2.2 (3,5 MB)
---
  V1.0 V1.1
 V14 / V14 SP1

Migrate TIA Portal V13 SP1 "Library V1.1" to TIA Portal V14/V14 SP1:
  Documentation V1.1 (3,6 MB)
 Registrierung notwendig  Library V1.1 (3,2 MB)

Migrate TIA Portal V13 SP1 "Library V2.1" to TIA Portal V14/V14 SP1:
  Documentation V2.1 (1,9 MB) 
 Registrierung notwendig  Library V2.1 (3,7 MB)

V13 SP1  Documentation V1.1 (3,6 MB)
 Registrierung notwendig  Library V1.1 (3,2 MB)
  Documentation V2.1 (1,9 MB)
 Registrierung notwendig  Library V2.1 (3,7 MB) 
V13  Documentation V1.0 (3,5 MB)
 Registrierung notwendig  Library V1.0 (4,1 MB)
---

Table 1

  • SIMATIC WinCC flexible & SIMATIC STEP 7 V5
    Contents of the library: function blocks for SIMATIC STEP 7 (SIMATIC S7-300/400),
    faceplates for SIMATIC WinCC flexible and screen windows for SIMATIC WinCC.
      
 Software versionSITOP PSU8600
firmware version
 STEP 7 WinCC  WinCC
 flexible
   V1.4
V5V7.52008Migrate library V2.4 to WinCC V7.5 
V5V7.42008  Documentation V2.4 (6,1 MB)
 Registrierung notwendig  Library V2.4.1 (3,0 MB)
 
V5V7.32008  Documentation V2.4 (6,1 MB)
 Registrierung notwendig  Library V2.4.0 (3,2 MB)
 
    V1.2 V1.3
V5V7.52008Migrate library V2.2 to WinCC V7.5.Migrate library V2.3 to WinCC V7.5
V5V7.4 2008  Documentation V2.2 (5,6 MB)
 Registrierung notwendig  Library V2.2.1 (3,0 MB) 
  Documentation V2.3 (5,6 MB)
 Registrierung notwendig  Library V2.3.1 (3,9 MB) 
V5V7.3 2008  Documentation V2.2 (5,6 MB)
 Registrierung notwendig  Library V2.2.0 (3,1 MB) 
  Documentation V2.3 (5,6 MB)
 Registrierung notwendig  Library V2.3.0 (4,0 MB) 
  V1.0V1.1
V5V7.4 / V7.52008Migrate library V1.0 to WinCC V7.4:
  Documentation V1.0 (1,8 MB)
 Registrierung notwendig  Library V1.0 (3,8 MB) 

Migrate library V2.1 to WinCC V7.4:

  Documentation V2.1 (6,1 MB)
 Registrierung notwendig  Library V2.1 (3,4 MB)

V5V7.32008Migrate library V1.0 to WinCC V7.3:
  Documentation V1.0 (1,8 MB)
 Registrierung notwendig  Library V1.0 (3,8 MB)

  Documentation V2.1 (6,1 MB)
 Registrierung notwendig  Library V2.1 (3,4 MB)
V5V7.22008  Documentation V1.0 (1,8 MB)
 Registrierung notwendig  Library V1.0 (3,8 MB) 
---

Table 2


Note
How to open and migrate libraries in TIA Portal can find under entry ID  37364723.
Information for migration of WinCC V7 libraries you can find under entry ID 44029132

The libraries for firmware V1.0 can be used under firmware V1.1 / V1.2 as well.

When using firmware V1.1 / V1.2 the usage of the libraries V2.1 / V2.2 or higher is recommended.
They enable the utilization of new functions provided by the firmware V1.1 / V1.2.

Further Information
SITOP Power Supplies in the Online Support
Support Packages for the hardware catalog in the TIA Portal (HSP)
GSD for SITOP PSU8600 for integration in SIMATIC STEP 7

Last Changes
Added new documentations and libraries V2.4 (STEP 7 V5.5, WinCC, WinCC flexible and TIA Portal (STEP 7, WinCC)) for firmware V1.4.

Additional Keywords
Panel, panels, faceplate, faceplates, UPS, buffer, buffering, brownout, temporary network failure, power cut

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit