×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 103433117, Entry date: 05/05/2020
(0)
Rate

Drives Software Version V4.7 HF35 for SINAMICS G130, SINAMICS G150 and SINAMICS S150

  • Entry
  • Associated product(s)
Here you can find the SINAMICS G130, SINAMICS G150 and SINAMICS S150 firmware version 4.7 HF35.

The version designation on the memory card (CF) is SINAMICS V04.07.00.35.

The internal firmware version number is SINAMICS V04.74.35.35.

When upgrading your system, please read the firmware update instructions. 


Restrictions SINAMICS G130, SINAMICS G150 and S150

The restrictions can be derived from the release note of SINAMICS S120 Firmware Version V4.7 HF35 (please refer to item 92522512)


SINAMICS Firmware Version 4.7 HF35

The following software can be downloaded:

SINAMICS G130 Firmware:

 Download unterliegt Exportcontrolle  Sinamics_G130_V_4_7_0_HF35.zip (66,3 MB)
Note: The software is subject to export restrictions. The download is only available to registered users.

Alternatively, you can use the new memory card(CF) which has following order number: 
6SL3054-3EH00-1BA0

SINAMICS G150 Firmware:

 Download unterliegt Exportcontrolle  Sinamics_G150_V_4_7_0_HF35.zip (68,3 MB)
Note: The software is subject to export restrictions. The download is only available to registered users.

Alternatively, you can use the new memory card(CF) which has following order number:
6SL3054-1EH00-1BA0

SINAMICS S150 Firmware:

 Download unterliegt Exportcontrolle  Sinamics_S150_V_4_7_0_HF35.zip (75,1 MB)
Note: The software is subject to export restrictions. The download is only available to registered users.

Alternatively, you can use the new memory card(CF) which has following order number: 
6SL3054-2EH00-1BA0 

GSD files for integrating projects in PROFIBUS engineering tools

On the Compact Flash Card, the PROFIBUS GSD files are stored in the following
path: ..\SIEMENS\SINAMICS\DATA\CFG
Alternatively the files can be downloaded: 98206128

GSDML  files for integrating projects in PROFINET engineering tools

On the Compact Flash Card, the PROFINET GSDML files are stored in the following
Path: ..\SIEMENS\SINAMICS\DATA\CFG
Alternatively the files can be downloaded: 98207877
   
STARTER

With the release of firmware version V4.7 HF35 the new STARTER Version 5.4 HF1 is also available (please refer to 26233208)

Startdrive / TIA Portal

SINAMICS G130, G150 and S150 with Profinet CU are supported in Startdrive V16.

For further information please see the announcement of the delivery release of SINAMICS Startdrive V16 (109771709) and in the commissioning manual for SINAMICS S120 (109771818).

DCC (Drive Control Chart)
(please refer to 109753687)   

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.