×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 103498563, Entry date: 10/27/2014
(2)
Rate

SIMOTION Print Standard for Corrugated Printing

  • Entry
  • Associated product(s)

Task
Modern corrugated machines consist of different modules with complex technological demands. These are for example feeder (servo or mechanical), printing unit, rotary die cutter and slotter.

Solution
This printing segment specific SIMOTION Scout project and document has its focus on the specific technology of corrugated printing machines. The application is based on the SIMOTION Print Standard V3.0.1 (see 38195516). The project contains the feeder, a printing unit, a slotter and a rotary die cutter.

The combination of the SIMOTION Print Standard and the library for corrugated printing supports a fast and successful implementation of SIMOTION in a corrugated printing machine project.

The project was created with Scout V4.4.

Note
If you are interested, please contact your local sales partner.
Contacts worldwide 

Additional search terms
motioncontrol_apc_applications, Wellpappe, corrugated board, Druck, Flexodruck, flexo printing

 

File

Date

 Registrierung notwendig  Manual_V1_0 (931,8 KB)

10/14

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.