×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 10351238, Entry date: 09/21/2010
(4)
Rate

How can you carry out an upgrade on an operating system that no longer supports the existing STEP 7 Micro/WIN version?

  • Entry
  • Associated product(s)

Instructions
Having STEP 7 Micro/Win installed on the PC is the requirement for a software upgrade. If you use an operating system (Windows 2000/XP/Vista) on which your existing STEP 7 Micro/Win version cannot run (you will find an overview of this in Entry ID: 8675614), then you will have to carry out a software upgrade of STEP 7 Micro/Win as described below.

  • Install the full version of the "old" STEP 7 Micro/Win on a supporting operating system (see Entry ID: 8675614)
  • Find the "microwin.exe" file (or "microdos.exe") with the Windows Explorer
  • Compress "microwin.exe" (or "microdos.exe") file (this is obligatory), for example with WinZip, and copy the file onto a mobile data carrier (disk, USB stick etc.)
  • Extract this file on your "new" operating system (Windows 2000/XP/Vista) in the same directory structure

You can begin with the STEP 7 Micro/Win software upgrade if the "microwin.exe" (or "microdos.exe") file is saved on your PC.

Keywords
Update, software installation, Windows, 95, 98, NT, 2000, XP, Vista

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.