×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 103528928, 文档发布日期 2015年5月11日
(8)
评估

Communication of a SIMATIC MV400 to a S7-1500 via PROFINET/IE

  • 文档
  • 涉及产品
For industrial identification purposes optical systems like SIMATIC MV400 are indispensable. This application example shows you how to operate the SIMATIC MV400 code reading system via PROFINET on a SIMATIC S7 automation system. In addition, some basic functions of the code reading system are shown.

Task
The SIMATIC MV400 code reading system is to be controlled via PROFINET through a SIMATIC S7-1200/1500 automation system.

Solution
In this application example we demonstrate how to operate the MV400 code reading system via PROFINET through a S7-1200/1500. In the enclosed STEP 7 project it is shown on an detailed example, how the code blocks of the STEP 7 “Identification” library can be used in order to realize the desired functionalities.

In order to clearly demonstrate the functionalities they can be operated via SIMATIC HMI Panel. In addition, a camera configuration file with predefined camera programs and settings and an adjusted CustomGUI (user-defined interface) is included as download.

The following basic functions are realized in this project by the blocks of the STEP 7 library:

  • RESET (initializing the code reader with program number specification, switching code reader to processing mode)
  • READ (reading trigger and result text, reading program number, reading match string)
  • WRITE (program change, enable single program number read, writing match string, enable single match string read)

The following additional functions of the code reading system are shown:

  • Displaying diagnostic screens (via SIMATIC HMI)
  • Loading/saving camera configuration (remote client via SIMATIC HMI)
  • Using user-defined interface (via SIMATIC HMI)

The following figure shows the pictorial schematic of this example application:

Downloads
  Documentation (2,3 MB)
 Registrierung notwendig  Project for SIMATIC S7-1200 with STEP 7 V15.1 (15,0 MB)
 Registrierung notwendig  Project for SIMATIC S7-1500 with STEP 7 V15.1 (15,2 MB)
 Registrierung notwendig  Configuration file for SIMATIC MV440 HR (8,4 MB)

 

Last Changes
Extension with SIMATIC S7-1200
Update TIA Portal V15.1

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.