×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 103528928, Entry date: 05/11/2015
(8)
Rate

Communication of a SIMATIC MV400 to a S7-1500 via PROFINET/IE

  • Entry
  • Associated product(s)
For industrial identification purposes optical systems like SIMATIC MV400 are indispensable. This application example shows you how to operate the SIMATIC MV400 code reading system via PROFINET on a SIMATIC S7 automation system. In addition, some basic functions of the code reading system are shown.

Task
The SIMATIC MV400 code reading system is to be controlled via PROFINET through a SIMATIC S7-1200/1500 automation system.

Solution
In this application example we demonstrate how to operate the MV400 code reading system via PROFINET through a S7-1200/1500. In the enclosed STEP 7 project it is shown on an detailed example, how the code blocks of the STEP 7 “Identification” library can be used in order to realize the desired functionalities.

In order to clearly demonstrate the functionalities they can be operated via SIMATIC HMI Panel. In addition, a camera configuration file with predefined camera programs and settings and an adjusted CustomGUI (user-defined interface) is included as download.

The following basic functions are realized in this project by the blocks of the STEP 7 library:

  • RESET (initializing the code reader with program number specification, switching code reader to processing mode)
  • READ (reading trigger and result text, reading program number, reading match string)
  • WRITE (program change, enable single program number read, writing match string, enable single match string read)

The following additional functions of the code reading system are shown:

  • Displaying diagnostic screens (via SIMATIC HMI)
  • Loading/saving camera configuration (remote client via SIMATIC HMI)
  • Using user-defined interface (via SIMATIC HMI)

The following figure shows the pictorial schematic of this example application:

Downloads
  Documentation (2,3 MB)
 Registrierung notwendig  Project for SIMATIC S7-1200 with STEP 7 V15.1 (15,0 MB)
 Registrierung notwendig  Project for SIMATIC S7-1500 with STEP 7 V15.1 (15,2 MB)
 Registrierung notwendig  Configuration file for SIMATIC MV440 HR (8,4 MB)

 

Last Changes
Extension with SIMATIC S7-1200
Update TIA Portal V15.1

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit