×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 103929354, Entry date: 12/12/2014
(0)
Rate

Delivery release for SINAMICS MICROMASTER STARTER V4.4 HF3 and additive SSPs

  • Entry
  • Associated product(s)
With this information, STARTER V4.4 HF3 incl. the additive SINAMICS Support Packages (SSP) SSP SINAMICS V4.7 SSP SINAMICS G120 V4.7 SSP SINAMICS G110M V4.6 SSP SINAMICS G110M V4.7 SSP SINAMICS G120P BT V4.7 SSP SINAMICS G120P V4.7 SSP SINAMICS SIMATIC ET200pro FC-2 V4.7 SSP SINAMICS integrated V4

With this information, STARTER V4.4 HF3 incl. the additive SINAMICS Support Packages (SSP)

  • SSP SINAMICS V4.7
  • SSP SINAMICS G120 V4.7
  • SSP SINAMICS G110M V4.6
  • SSP SINAMICS G110M V4.7
  • SSP SINAMICS G120P BT V4.7
  • SSP SINAMICS G120P V4.7
  • SSP SINAMICS SIMATIC ET200pro FC-2 V4.7
  • SSP SINAMICS integrated V4.7
  • SSP SINAMICS MV V4.7

has been released for delivery.

Update: 12/12/2014

Important hint according the STARTER V4.4 Hotfix 3 together with SINUMERIK

Please do not use the STARTER V4.4 Hotfix 3 release together with SINUMERIK devices. Please still use the STARTER version V4.4.

If the SINUMERIK user already have installed the Hotfix 3 version of STARTER, please go back and reinstall the STARTER Version V4.4. If there will be a problem with the availability of the STARTER Version V4.4, please contact your SIEMENS partner.

STARTER V4.4 HF3 is backward compatible with the previous STARTER versions and replaces these.

The following drive systems are supported (newly added versions are shown in bold):

  • MICROMASTER 4th generation (MM420 V1.30, MM440 V2.20, MM430 V2.20)

  • SINAMICS DCM with firmware V1.1, V1.2, V1.3 and (with SSP) V1.4

  • SIMATIC ET200S FC with firmware V1.0.x, V3.0.x

  • SIMATIC ET200pro FC with firmware V3.0.x, V3.1.x

  • SINAMICS SIMATIC ET200pro FC-2 with firmware (with SSP) V4.7

  • SINAMICS G110 with firmware V1.0.x, V1.1.x, 1.2.x

  • SINAMICS G110M with firmware(with SSP) V4.6 and V4.7

  • SINAMICS G110D with firmware V3.3.x, V3.4.x, V3.6.x

  • SINAMICS G120 with firmware V2.0.x, V2.1.x, V3.0.x, V3.1.x, V3.2.x

  • SINAMICS G120 with firmware V4.2, V4.3.0, V4.3.2, V4.4, V4.5, V4.6 and (with SSP) V4.7

  • SINAMICS G120C with firmware V4.4, V4.5, V4.6 and (with SSP) V4.7

  • SINAMICS G120D with firmware V3.0.x, V3.1.x, V3.2.x, V4.5, V4.6 and (with SSP) V4.7

  • SINAMICS G120P with firmware V4.2, V4.3.0, V4.3.2, V4.4, V4.5, V4.6 and (with SSP) V4.7

  • SINAMICS G120P BT with firmware V4.4.1, V4.6 and (with SSP) V4.7

  • SINAMICS G130 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2

  • SINAMICS G130 with firmware V4.3.1, V4.3.2, V4.4, V4.5, V4.6 and (with SSP) V4.7

  • SINAMICS G150 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2

  • SINAMICS G150 with firmware V4.3.1, V4.3.2, V4.4, V4.5, V4.6 and (with SSP) V4.7

  • SINAMICS GM150 with firmware V2.5.1, V2.6.1 and V2.6.2

  • SINAMICS GL150 with firmware V2.5.1, V2.6.1 and V2.6.2

  • SINAMICS GL150 with firmware V4.3.1, V4.4.2, V4.5 (--> SINAMICS MV)

  • SINAMICS S110 with firmware V4.1, V4.3.1, V4.3.2, V4.4

  • SINAMICS S120 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2

  • SINAMICS G120 with firmware V4.3.1, V4.3.2, V4.4, V4.5, V4.6 and (with SSP) V4.7

  • SINAMICS S150 with firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2

  • SINAMICS G150 with firmware V4.3.1, V4.3.2, V4.4, V4.5, V4.6 and (with SSP) V4.7

  • SINAMICS SL150 with firmware V4.3.1, V4.4.2, V4.5 (--> SINAMICS MV)

  • SINAMICS SM120 with firmware V4.4.2 (--> SINAMICS MV)

  • SINAMICS MV (GM150/GL150/SL150/SM120) with firmware V4.6 and (with SSP) V4.7

Further details on the supported drive systems can be found in the following Excel overview:

The following error corrections are available in version V4.4 HF3 when compared to the previous version V4.4:

  • Cross-device STARTER expanded functionality

    • In the case of a PC with a time zone setting in Windows with a negative sign (e.g. UMC/GMT -01:00 or -02:00 or -03:00, etc.), saved trace files (*.trc) cannot be opened with STARTER. (TFS 335569)
  • SINAMICS S120, G130, G150, S150
    • Removed restriction in conjunction with upgrading SINAMICS drives (CU320-2 with PROFINET) from firmware V4.4 to a current firmware version in conjunction with the use of PROFIsafe telegrams:
      After upgrading the firmware of the CU, the alarm "A01796 (F, N) SI (CU): Waiting for communication (3)" is displayed on some drives, and PROFIsafe communication does not take place. (TFS 334721)
    • The device name of Ethernet changes when the function "Save and compile" is activated in the hardware configuration of STEP 7 on SINAMICS drives with CU320-2 with PROFINET. The cause is the change to the SINAMICS device name in the STARTER project by operating the STARTER functions. (TFS 329460)
  • SINAMICS G110/G110M/G120-2/G120C/G120D-2/G120P

    • SINAMICS G120 with PROFINET and STEP 7 HW Config:
      • The following error behavior has been corrected:
        Drive commissioning is performed in online mode; then the device data is loaded to the project. The device name is changed in the offline project and therefore the existing device name is modified and overwritten in the STEP 7 project. After downloading the HW configuration again, the project no longer runs. (TFS 324295)

Information about SINAMICS DCC V2.3

Information about SINAMICS DCC V2.3 for STARTER V4.4 HF3 and firmware versions can be found under 98206100.

Installation versions

STARTER can be operated in the following installation versions:

  • STARTER Standalone

  • STARTER integrated in STEP 7 for applications with SIMATIC S7

  • STARTER integrated in SIMOTION SCOUT or SIMATIC S7 technology

Sources of supply for SINAMICS MICROMASTER STARTER

  • This (the current) STARTER version can be ordered under the order number (MLFB) 6SL3072-0AA00-0AG0 on DVD incl. the license certificate. A nominal charge of € 28.86 is incurred for order processing.
  • This current STARTER version (V4.4 HF3 or more recent) can also be downloaded under 26233208. The download can be used by anyone who already has a STARTER license certificate of any version.
  • STARTER V4.4 HF3 will be included in a following SIMOTION SCOUT V4.4 hotfix.

SINAMICS MICROMASTER STARTER can be used free of charge.

Information about the installation and the opening of existing projects

STARTER V4.4 HF3 can only be installed with administrator rights on the PG/PC. User rights are sufficient to operate STARTER (exception: Adding additional PG/PC interfaces).

STARTER V4.4 HF3 only has one setup for both installation versions ("STARTER Standalone" and "STARTER DriveES").

  • If no STEP 7 is available, the standalone versions will be installed on your computer.
  • If there is a STEP 7 installation on your computer, the Drive ES version will be installed/updated. (Note: Drive ES Basic must no longer be installed as a prerequisite (as of STARTER V4.3 SP2!)).


Support

A Guided Tour can be downloaded which facilitates familiarization with the STARTER (see 21110668).

Note on STARTER and other engineering software

Simultaneous operation of the STARTER, SIMOTION SCOUT and SIMATIC S7-Technology versions in a shared partition on one PG/PC is not supported. STARTER and Startdrive V12, V12 SP1 or V13 can be installed in parallel on a shared partition and operated simultaneously.

Important note for installation in context with SIMATIC PCS 7:
SIMATIC PCS 7 CiR capability (configuration in run) for existing projects with Siemens drives at PROFIBUS DP or PROFINET IO

Affected User/Project Scenario

The loss of the CiR capability of SIMATIC PCS 7 can be caused by the following SW update:

- Installation of this new STARTER version

This installation often also update the software components SlaveOM (PROFIBUS DP) and DeviceOM (PROFINET IO). If the existing configuration is translated afterwards, then the internal configuration data are changed due to the version and the generated configuration data will sometimes cause a loss of CiR capability!

Please check that the current configuration can be loaded via "Station > Check CiR Capability" at HW-Config.

Remedy

Information in detail according the CiR capability you find at the System Manual “PCS 7 Process Control System CPU 410 Process Automation”. These "changed" configuration data must be loaded once in the STOP state of the CPU and then CiR Capability for further translations and loading processes is available again.

If this procedure is not possible with your system, please contact the Customer Service.

Minimum system requirements

The following minimum requirements must be met:

  • Hardware
    • PG or PC with Pentium III min. 1 GHz (recommended > 1 GHz)
    • 1 GB working memory (2 GB recommended)
    • Screen resolution 1024 × 768 pixels, 16-bit color depth
    • Free hard disk memory: > 3 GB
  • Software
    • Microsoft Internet Explorer as of V6.0
    • 32-bit operating systems
      • Microsoft Windows Server 2003 SP2
      • Microsoft Windows XP Professional SP3*)
      • Microsoft Windows 7 Professional SP1
      • Microsoft Windows 7 Ultimate SP1
      • Microsoft Windows 7 Enterprise SP1 (standard installation)
    • 64-bit operating systems
      • Microsoft Windows 7 Professional SP1
      • Microsoft Windows 7 Ultimate SP1
      • Microsoft Windows 7 Enterprise SP1 (standard installation)
      • Microsoft Windows Server 2008 R2 SP1

*): Note: The release of STARTER with Windows XP will no longer be possible in future STARTER versions.

The STARTER setup can only be performed for "native" Windows versions with Far Eastern languages when an MUI version of Windows XP or Windows 7 is used. The executability in a software configuration other than the one above has not been tested.

Supported languages

  • German
  • English
  • French
  • Italian
  • Spanish

For further information please contact your Siemens Personal Contact.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.