×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 104020669, Entry date: 12/16/2014
(4)
Rate

SINAMICS S120/S150: Release for delivery, license for high output frequency

  • Entry
  • Associated product(s)
Effective immediately, SINAMICS S120/S150 license 'high output frequency' is released for general availability. ...

Effective immediately, SINAMICS S120/S150 license "high output frequency" is released for general availability.

Content

1. New licenses: High output frequency

2. Components involved

1. New license: High output frequency

The "High output frequency" license

  • Allows users to withdraw the output frequency limit if, as a result of the application, output frequencies of more than 550 Hz are required.
  • It is available under Article No. 6SL3074-0AA02-0AA0:

The "High output frequency" license can also be ordered together with the CF card by specifying Z option J01. This license is then permanently assigned to this CF card. Z option J01 is only available for SINAMICS S120 and S150.

The license is valid for SINAMICS S120 and S150 from firmware version V4.7 HF7 for Control Units:

  • CU320-2 DP (Article No. 6SL3040-1MA00-0AA0)
  • CU320-2 PN (Article No. 6SL3040-1MA01-0AA0)
  • CU310-2 DP (Article No. 6SL3040-1LA00-0AA0)
  • CU310-2 PN (Article No. 6SL3040-1LA01-0AA0)

The change to the EC Dual Use regulation has been ratified. This results in more stringent export regulations for converter systems, from SINAMICS firmware version V4.7 HF7 and higher for SINAMICS S120 / S150 for the CU320-2 and CU310-2 Control Units, the output frequency is limited to 550 Hz.

The "High output frequency" license

  • can be individually ordered under Article No. 6SL3074-0AA02-0AA0 and must then be assigned to a CF card using the WEB License Manager (www.siemens.com/automation/license).
  • it can also be ordered together with the CF card by specifying Z option J01. This license is then permanently assigned to this CF card.
  • is subject to export restrictions, and has export code: AL:3E225, ECCN: N SH code: 0.

2. Components involved

The change to the EC Dual Use regulation has been ratified. This results in more stringent export regulations for converter systems, from SINAMICS firmware version V4.7 HF7 and higher for SINAMICS S120 / S150 for the CU320-2 and CU310-2 Control Units, the output frequency is limited to 550 Hz.

Control Units involved:

  • CU320-2 DP (Article No. 6SL3040-1MA00-0AA0)
  • CU320-2 PN (Article No. 6SL3040-1MA01-0AA0)
  • CU310-2 DP (Article No. 6SL3040-1LA00-0AA0)
  • CU310-2 PN (Article No. 6SL3040-1LA01-0AA0)

The version designation on the Compact Flash card is SINAMICS S120 V04.07.00.07. The internal version number of the firmware is SINAMICS S120 V04.70.35.16.

The article numbers are as follows:

  • 6SL3054-0EH00-1BA0:
    Compact flash card 2 GB with firmware V4.7 without firmware option performance extension
  • 6SL3054-0EH01-1BA0:
    Compact Flash Card 2 Gb with firmware V4.7 incl. Firmware option, performance extension

Impact on the AL export code (export list number):

Component

Up to now

New

SINAMICS firmware ≥ V4.7 HF7 (where the output frequency is limited)

AL: 9I999

AL: N

SINAMICS firmware < V4.7 HF7 (where the output frequency is not limited)

AL: 9I999

AL: 3D225

The firmware version V4.7 can be obtained from the following sources as a download:

  • 92522512
  • PridaNet (only for Siemens service personnel)

Note

The SINAMICS S120 firmware version V4.7 can only be installed on the 1 GB and 2 GB compact flash cards of the CU310-2/CU320-2. Compact flash cards of the older CU310/CU320 cannot be used with firmware version V4.7.

Notes

  • For SIMOTION D (SINAMICS Integrated), the following applies:
    • When using SIMOTION D firmware with a SINAMICS Integrated from V4.7 HF7 and higher, for an output frequency greater than 550 Hz, the "High output frequency" license is required; for additional details, see 104020777.
  • For SINUMERIK (SINAMICS Integrated) the following applies:
    • None of the SINUMERIK software versions have any export restrictions regarding a high output frequency. Also future SINUMERIK software versions are not affected by this regulation, and are not limited to 550 Hz.
  • For SINAMICS S110 from V4.4 SP3, the output frequency will be permanently limited to 550 Hz; this will not be able to be withdrawn with a license.
  • For SINAMICS G120, already from V4.7 HF3 and higher, the output frequency is limited to 550 Hz. It cannot be withdrawn using a license.
Further information

Additional information on this topic is available in the fact sheet from the German Ministry for the Economy and Export Monitoring http://www.bafa.de/ausfuhrkontrolle/de/arbeitshilfen/merkblaetter in the "Fact sheet for exporting frequency converters".


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.