×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 104427619, Entry date: 11/25/2014
(0)
Rate

Update 1 for SIMATIC WinAC RTX 2010 SP2 and SIMATIC WinAC RTX F 2010 SP2 Released for Delivery

  • Entry
  • Associated product(s)

Update 1 for SIMATIC WinAC RTX 2010 SP2 and SIMATIC WinAC RTX F 2010 SP2 is herewith released for delivery.

Update 1 will provide the following corrections for SIMATIC WinAC RTX (F) 2010 SP2:

  • Upload to the target system not possible
    In rare cases an upload from STEP 7 V5.5 by means of the menu command "Target System > Load Station to PG" was not possible. The following message would appear: "The configuration cannot be uploaded to the PG, because it cannot be determined from the CPU."

    WinAC RTX (F) 2010 SP2 Update 1 will now enable the upload to the target system.
  • Debug functionality is not fully available (TIA Portal)
    Monitoring in the TIA Portal will sometimes not show all values.

    With WinAC RTX (F) 2010 SP2 Update 1 you can now make full use of the debug functionality in the TIA Portal.
    Depending on the structure of the PLC program not all successive process values can sometimes be depicted in one display window. For this reason it is now possible to select individual actual values in a window, for display purposes. You can select the actual values in the program editor for this purpose. In the context menu command select "Control" -> "Monitor the selection".

  • Project cannot be loaded twice (TIA Portal)
    If you wish to upload a project without any changes to the CPU a second time, it can happen that the Controller Panel of WinAC RTX will refuse to respond and the PC cannot be cold restarted correctly. 

    With WinAC RTX (F) 2010 SP2 Update 1 you can now upload an unchanged project to the CPU as often as you wish.

Installation instructions: 

To be able to install Update 1 the SP2 for WinAC RTX 2010 or WinAC RTX F 2010 must have been installed beforehand. For enhancements, new functions and availability of the SP2 see entry ID 99005716

Please note:
During the installation the settings for the storage path of the program and configuration files will be reset to the default settings. Please correct these paths if you have made individual settings.

Availability

To obtain the Update 1 for WinAC RTX 2010 SP2 or WinAC RTX F 2010 SP2 please contact our Technical Support under:

By telephone: +49 911 895 7222
Via Internet: http://support.automation.siemens.com   

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit