×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 104946406, Entry date: 01/18/2019
(8)
Rate

Which technical data applies for the SIMATIC Modbus/TCP blocks and for which CPUs and CPs is it released?

  • Entry
  • Associated product(s)
This entry provides the technical data of the SIMATIC Modbus/TCP blocks and information about the CPUs and CPs for which the SIMATIC Modbus/TCP blocks are released.

Description
The following technical data applies for the SIMATIC Modbus/TCP blocks.

  1. Client/Server
    Both Server mode and Client mode are supported. With the Server mode you should note that not all SIMATIC CPUs with integrated PROFINET interface support the local Port 502 for communication. With Modbus/TCP PAC the CPU functions exclusively as Client.
  2. Modbus services according to specification
    The "SIMATIC Modbus/TCP CP", "SIMATIC Modbus/TCP PN", "SIMATIC Modbus/TCP PN Red" and "SIMATIC Modbus/TCP Red" products support function codes 1, 2, 3, 4, 5, 6, 15 and 16.
    The "SIMATIC Modbus/TCP PAC" product reads out the values of the base type 3 and the energy meters.
  3. PCS 7
    The Modbus/TCP blocks are PCS7 conform. All Modbus/TCP blocks are released for PCS 7 V7.1, PCS 7 V8 and PCS 7 V9.x. The sample CFC projects were created with PCS 7 V7.1 SP2 and PCS 7 V8 respectively.
  4. Redundancy
    Blocks with the Redundancy function provide the option of establishing redundant communication. If a connection breaks down, the block automatically switches to another connection (can be parameterized in "SIMATIC Modbus/TCP CP Red" and "SIMATIC Modbus/TCP PN Red"). The blocks run here in Hot Standby mode. Unilateral or bilateral redundancy can be established depending on the partner.
  5. Method
    Native TCP connections are established for Modbus communication between SIMATIC stations and other Modbus devices. Here the standard functions of the SIMATIC S7 library are used (AG_SEND and AG_RECV for communication via CP, T blocks for communication via the integrated PROFINET interface of the CPU). All Modbus/TCP blocks are multi-instance capable.
  6. Licensing
    The license is CPU-specific. The license cannot be transferred from one CPU to another. No license is needed for testing.

SIMATIC Modbus/TCP CP and SIMATIC Modbus/TCP CP Red
Table 2 shows the CPs for which the following products are released.

ProductArticle numberFirmware version of the CPU used / Note 
SIMATIC Modbus/TCP CP
  • 6AV6676-6MB00-6AX0 (packet)
  • 6AV6676-6MB00-6AD0 (download)

  • S7-300 CPUs FW V3.2 and higher
  • S7-400 CPUs FW V6.0 and higher
2XV9450-1MB00
If you are using an S7-300 CPU with FW < V3.2 or an S7-400 CPU with FW < V6.0, then you have to use the predecessor version 2XV9450-1MB00.
SIMATIC Modbus/TCP CP Red
  • 6AV6676-6MB30-4AX0 (packet)
  • 6AV6676-6MB30-4AD0 (download)

  • S7-300 CPUs FW V3.2 and higher
  • S7-400 CPUs FW V6.0 and higher
  • 6AV6676-6MB30-3AX0 (packet)
  • 6AV6676-6MB30-3AD0 (download)
If you are using an S7-300 CPU with FW < V3.2 or an S7-400 CPU with FW < V6.0, then you have to use the predecessor version 6AV6676-6MB30-3AX0 or 6AV6676-6MB30-3AD0.

 Table 1
 

HardwareArticle numberFirmware version
CP 343-1 Lean6GK7343-1CX10-0XE01)V2.1 and higher
CP 343-1 Standard6GK7343-1EX21-0XE0V1.0.17 and higher
6GK7343-1EX30-0XE01)V2.0.16 and higher
CP 343-1 Advanced6GK7343-1GX21-0XE0V1.0.24 and higher
6GK7343-1GX30-0XE0V1.0.23 and higher
6GK7343-1GX31-0XE0V3.0 and higher
CP 443-1 Standard6GK7443-1EX20-0XE0V1.0.26 and higher, but not V2.1.12
6GK7443-1EX30-0XE01)V3.0 and higher, but not V3.2.9
6GK7443-1EX30-0XE11)
CP 443-1 Advanced6GK7443-1EX40-0XE0V2.2.35 and higher
6GK7443-1EX41-0XE0V1.0.24 and higher
6GK7443-1GX20-0XE0V2.0 and higher, but not V2.1.12
6GK7443-1GX30-0XE01)V3.0 and higher but not V3.2.9

Table 2

1) These CPs support the multiple Port 502. When using SIMATIC Modbus/TCP CP V4.3 you must use the blocks with FC10 "AG_CNTRL" (from the Current directory).

Note the amount of local data required for the Modbus block. Refer to the technical data of your CPU for the available local data.
The products "SIMATIC Modbus/TCP CP" and "SIMATIC Modbus/TCP CP Red" are released for Standard CPUs, F CPUs and H CPUs.

SIMATIC Modbus/TCP PN and SIMATIC Modbus/TCP PN Red
The following products can be used for ET 200S CPUs, ET 200pro, S7-300 CPUs and S7-400 CPUs with integrated PROFINET interface.

ProductArticle numberFirmware version of the CPU used / Note 
SIMATIC Modbus/TCP PN
  • 6AV6676-6MB20-3AX0 (packet)
  • 6AV6676-6MB20-3AD0 (download)

  • S7-300 CPUs FW V3.2 and higher
  • S7-400 CPUs FW V6.0 and higher
  • ET 200 CPUs FW V3.2 and higher
2XV9450-1MB02
If you are using an S7-300 CPU < FW V3.2, an S7-400 CPU < FW V6.0 or WinAC RTX, you have to use the predecessor version 2XV9450-1MB02.
SIMATIC Modbus/TCP PN Red
  • 6AV6676-6MB10-0AX0 (packet)
  • 6AV6676-6MB10-0AD0 (download)

Table 3 

Information about released ports of the PN CPUs is available in Entry ID 34010717.

SIMATIC Modbus/TCP SENTRON PAC
The following products can be used for ET 200S CPUs, S7-300 CPUs and S7-400 CPUs with integrated PROFINET interface.
 

ProductArticle number 
SIMATIC Modbus/TCP 20 SENTRON PAC6AV6676-6MA30-0AX0
SIMATIC Modbus/TCP 100 SENTRON PAC6AV6676-6MA30-1AX0
SIMATIC Modbus/TCP 512 SENTRON PAC 6AV6676-6MA30-2AX0

Table 4
 

HardwareNote
PAC 3200V2.2.1 and higher
PAC 4200V1.5.1 and higher

Table 5

Information about released ports of the PN CPUs is available in Entry ID 34010717.

Additional Keywords
Loadable drivers, Communication blocks, Modbus, Redundancy

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.