×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 105128409, Entry date: 02/27/2015
(10)
Rate

DOConCD: Installation on Windows 7 with Adobe Reader X and higher

  • Entry
  • Associated product(s)
By installing an additional tool, DOConCD up to edition 03/2013 can also run on Adobe Reader X and higher with a somewhat restricted functional scope. Following editions are not affected because of the change of the software tool.

Question
How can DOConCD up to edition 03/2013 be used with Adobe Reader X and higher?

Answer
In order that DOConCD runs on Adobe Reader X and higher, you require a plug-in, which adapts the installation to the more stringent security requirements of Adobe Readers X. As a consequence, some functions are no longer available (e.g. saving favorites).

The workaround to install DOConCD encompasses 3 steps:

  1. Install setup for DOConCD in the recommended directories.
  2. Download a new setup (AddOn_DOConCD_AdobeReaderX.zip ( 732 KB ) ) and unzip in any directory.
  3. Start the setup from the directory.

You can find details on the installation readme ( 90 KB ) in the attachment.
Additional information about the documentation is available at: http://www.siemens.com/motioncontrol/docu.

  Liesmich_AddOn_DOConCD_fuer_AdobeReaderX.pdf ( 92 KB )
  Readme_AddOn_DOConCD_for_AdobeReaderX_en.pdf ( 90 KB )

  AddOn_DOConCD_AdobeReaderX.zip ( 732 KB )

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit