Entry type: Download, Entry ID: 105825934, Entry date: 01/22/2015
(169)
Rate

Service Pack 1 for SIMATIC STEP 7 V13 incl. PLCSIM (TIA Portal)

  • Entry
  • Associated product(s)

The Service Pack is applicable to the following products:

  • STEP 7 Professional V13
  • STEP 7 Basic V13

New features and changes compared to earlier versions are described in the delivery release for STEP 7 V13 SP1: 103627307

Important installation instructions:
Installation of the Service Pack requires prior installation of the STEP 7 V13 software.

The TIA Portal products STEP 7 (incl. PLCSIM), Safety, WinCC and Startdrive must be updated to the same version (V13 SP1). SIMOTION SCOUT TIA also must be updated to version V4.4 HF5. 
If the versions differ, the TIA Portal can no longer be started. Please ensure that you have the Service Packs for these products on hand before you begin with the installation. The Service Packs are available from the following entry bulletins:


Instructions for the download 

The download is divided into several files. Please download all the files into the same directory and execute the file ending with .exe. The files will now be combined and you can execute the setup.

Servicepack 1 for STEP 7 V13 Professional

 SIMATIC_STEP_7_Professional_SP1_for_V13.exe (2714 KB) ( 2714 KB )
SIMATIC_STEP_7_Professional_SP1_for_V13.001 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Professional_SP1_for_V13.002 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Professional_SP1_for_V13.003 (665600 KB) ( 665600 KB )  
SIMATIC_STEP_7_Professional_SP1_for_V13.004 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Professional_SP1_for_V13.005 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Professional_SP1_for_V13.006 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Professional_SP1_for_V13.007 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Professional_SP1_for_V13.008 (665600 KB) ( 665600 KB )

SIMATIC_STEP_7_Professional_SP1_for_V13.009 (665600 KB) ( 665600 KB )  

SIMATIC_STEP_7_Professional_SP1_for_V13.010 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Professional_SP1_for_V13.011 (338220 KB) ( 338220 KB )

 

Servicepack 1 for STEP 7 V13 Basic

 

SIMATIC_STEP_7_Basic_SP1_for_V13.exe (2714 KB) ( 2714 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.001 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.002 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.003 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.004 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.005 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.006 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.007 (665600 KB) ( 665600 KB )

 SIMATIC_STEP_7_Basic_SP1_for_V13.008 (665600 KB) ( 665600 KB )

SIMATIC_STEP_7_Basic_SP1_for_V13.009 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.010 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V13.011 (87512 KB) ( 87512 KB )

 Servicepack 1 for STEP 7 PLCSIM V13 (STEP 7 Basic and STEP 7 Professional)

 

SIMATIC_S7_PLCSIM_V13_SP1.exe (2596 KB) ( 2596 KB )

SIMATIC_S7_PLCSIM_V13_SP1.001 (665600 KB) ( 665600 KB )
SIMATIC_S7_PLCSIM_V13_SP1.002 (616608 KB) ( 616608 KB )