×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 106313733, Entry date: 11/27/2014
(0)
Rate

SITRANS LR250 HEA. Should the SITRANS LR250 Hygienic Encapsulated Antenna be used in applications which can see build up?

  • Entry
  • Associated product(s)

Question:
Should the SITRANS LR250 Hygienic Encapsulated Antenna be used in applications which can see build up?

Answer:
High frequency radar can suffer more so than lower frequency radar, so some applications with heavy build up may require some cleaning. It is also not advisable to have prolonged build up in hygienic/sanitary applications as this could introduce contamination. Condensation can regularly be ignored by SITRANS LR250 due to its dynamic echo processing within Process Intelligence. 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.