×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 106567433, Entry date: 01/22/2015
(98)
Rate

Service Pack 1 for SIMATIC WinCC V13 (TIA Portal)

  • Entry
  • Associated product(s)

The Service Pack is applicable to the following products:

  • WinCC Basic V13
  • WinCC Comfort V13
  • WinCC Advanced V13
  • WinCC Professional V13
  • WinCC Runtime Advanced V13
  • WinCC Runtime Professional / Client V13
  • WinCC Runtime Professional / Client ASIA V13

New features and changes compared to earlier versions are described in the delivery release for WinCC V13 SP1 (entry ID 104509915

 

Important installation instructions:

To be able to install the Service Pack the WinCC V13 software must be installed already.

 

The TIA Portal products STEP 7 (incl. PLCSIM), Safety, WinCC and Startdrive must be upgraded to the same version (V13 SP1). SIMOTION SCOUT TIA also must be updated to version V4.4 HF5.
If the versions differ, the TIA Portal can no longer be started. Please ensure that you have the Service Packs of these products on hand before you start with the installation. The Service Packs are available under the following entry IDs:

 

Download 

The download is subdivided into several files. Please download all the files into the same folder and then execute the file ending with .exe. The parts will then be combined and you can execute the setup.  

 

WinCC Basic
Free download of Service Pack 1 for WinCC Basic V13.

This free download contains the Service Pack 1 for upgrading existing installations of WinCC Basic V13 and can only be installed, if WinCC Basic V13 is installed already.

SIMATIC_WinCC_Basic_SP1_for_V13.exe ( 2714 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.001 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.002 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.003 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.004 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.005 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.006 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.007 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.008 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.009 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.010 ( 665600 KB )

SIMATIC_WinCC_Basic_SP1_for_V13.011 ( 273674 KB )


WinCC Comfort/Advanced
Free download of Service Pack 1 for WinCC Comfort/Advanced V13.

This free download contains the Service Pack 1 for upgrading existing installations of WinCC Comfort/Advanced V13 and can only be installed, if WinCC Comfort/Advanced V13 is installed already.

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.exe ( 2714 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.001 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.002 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.003 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.004 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.005 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.006 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.007 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.008 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.009 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.010 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.011 ( 665600 KB )

SIMATIC_WinCC_Comfort_Advanced_SP1_for_V13.012 ( 426343 KB )


WinCC Professional
Free download of Service Pack 1 for WinCC Professional V13.

This free download contains the Service Pack 1 for upgrading existing installations of WinCC Professional V13 and can only be installed, if WinCC Professional V13 is installed already.

SIMATIC_WinCC_Professional_SP1_for_V13.exe ( 2714 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.001 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.002 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.003 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.004 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.005 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.006 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.007 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.008 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.009 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.010 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.011 ( 665600 KB )

SIMATIC_WinCC_Professional_SP1_for_V13.012 ( 633932 KB )


WinCC Runtime Advanced
Free download of Service Pack 1 for WinCC Runtime Advanced V13.

This free download contains the Service Pack 1 for upgrading existing installations of  WinCC Runtime Advanced V13 and can only be installed, if WinCC Runtime Advanced V13 is installed already.

SIMATIC_WinCC_Runtime_Advanced_SP1_for_V13.exe ( 1093781 KB )


WinCC Runtime Professional / Client (ASIA)
Free download of Service Pack 1 for WinCC Runtime Professional V13.

This free download contains the Service Pack 1 for upgrading existing installations of  WinCC Runtime Professional / Client (ASIA) V13 and can only be installed, if WinCC Runtime Professional / Client (ASIA) V13 are installed already.

SIMATIC_WinCC_Runtime_Professional_SP1_for_V13.exe ( 2713 KB )

SIMATIC_WinCC_Runtime_Professional_SP1_for_V13.001 ( 665600 KB )

SIMATIC_WinCC_Runtime_Professional_SP1_for_V13.002 ( 665600 KB )

SIMATIC_WinCC_Runtime_Professional_SP1_for_V13.003 ( 665600 KB )

SIMATIC_WinCC_Runtime_Professional_SP1_for_V13.004 ( 665600 KB )

SIMATIC_WinCC_Runtime_Professional_SP1_for_V13.005 ( 665600 KB )

SIMATIC_WinCC_Runtime_Professional_SP1_for_V13.006 ( 639604 KB )

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.