×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 10678936, Entry date: 08/25/2011
(0)
Rate

Why do I get a license error message in SIMATIC PDM although all the necessary licenses are available?

  • Entry
  • Associated product(s)

Description:
A license error message from SIMATIC PDM can basically have three reasons:

  1. Authorizations are available, but are not recognized. This is extremely rare. In this case you have to play the licenses back to the floppy disk, restart the computer and transfer the licenses back again from the floppy disk to the computer.
  1. The license for SIMATIC PDM is indeed available, but it is not the right version. The license for SIMATIC PDM Standalone must always be installed. It is a basic license and the only one that has to be updated with a new version of SIMATIC PDM. Below is a list of the licenses of SIMATIC PDM Standalone specifying the associated version of SIMATIC PDM:

Designation of the authorization

Valid for:

SIK/SIMATIC PDM Basis Standalone

Versions of PDM before PDM V5.0.1.

SIK/SIMATIC PDM Basis Standalone V5

PDM V5.0.1. / PDM V5.0.2. (+SP1)

SIK/SIMATIC PDM Basis Standalone V5.1

PDM V5.1 (+SP1 / +SP2)

SIK/SIMATIC PDM Basis Software V5.2

PDM V5.2

  1. Options for PDM are being used for which there is no license available. Below is indicated when an options license has to be installed:

Designation of the authorization

Authorized function:

Restrictions/
Special features

SIK/SIMATIC PDM Basis Integrated

Integration in SIMATIC STEP 7
up to PDM V5.1 with installed STEP 7
PDM V5.2 and higher with devices that are integrated in the HW Configuration

 

SIK/SIMATIC PDM Routing

If access is to be made to field devices beyond network boundaries (routing)

Only possible integrated in STEP 7
(-> Authorization for SIK/SIMATIC PDM Basis Integrated necessary)

SIK/SIMATIC PDM PROFIBUS DP/PA

If DP or PA devices are to be addressed/parameterized

In SIMATIC PDM V5.2 and higher this functionality is integrated in the basic software. No authorization is necessary.

SIK/SIMATIC PDM HART Mux

When implementing HART multiplexers

 

SIK/SIMATIC PDM ET 200 HART

When connecting HART devices to an ET 200M

In SIMATIC PDM V5.1 and higher this functionality is integrated in the basic software. No authorization is necessary.

SIK/SIMATIC PDM Tag Count unlimited

For parameterizing an unlimited number of field devices

Not for SIMATIC PDM V5.1

SIK/SIMATIC PDM max. 128 Tags

For parameterizing a maximum of 128 field devices

 

SIK/SIMATIC PDM max. 512 Tags

For parameterizing a maximum of 512 field devices

 

SIK/SIMATIC PDM max. 1024 Tags

For parameterizing a maximum of 1024 field devices

Available in SIMATIC PDM V5.1 and higher

SIK/SIMATIC PDM max. 2048 Tags

For parameterizing a maximum of 2048 field devices

Available in SIMATIC PDM V5.1 and higher

SIK/SIMATIC PDM max. 4096 Tags

For parameterizing a maximum of 4096 field devices

Only in SIMATIC PDM V5.1

SIK/SIMATIC PDM max. 8192 Tags

For parameterizing a maximum of 8192 field devices

Only in SIMATIC PDM V5.1

SIK/SIMATIC PDM max. 16384 Tags

For parameterizing a maximum of 16384 field devices

Only in SIMATIC PDM V5.1

SIK/SIMATIC PDM Diagnosis

For license error messages please see also FAQ 10308008

Option is discontinued

Notes:
For the "Data Record Routing" function the automation system must be equipped with communications processors CP 443-5 Extended (CP 443-5DX02 with FW 3.0 or higher) and CP 443-1 (CP 443-1EX02 or higher). Please refer also to FAQ ID 7808062. Options licenses for earlier versions of SIMATIC PDM remain valid. 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit