×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 107586911, Entry date: 01/29/2015
(10)
Rate

SIMOTION SCOUT, SCOUT standalone and SCOUT TIA V4.4 HF4

  • Entry
  • Associated product(s)
Download des Hotfix 4 zu SIMOTION SCOUT, SCOUT Stand-alone und SCOUT TIA V4.4 HF2

Attached you will find hotfix 4 for the engineering system SIMOTION SCOUT, SCOUT standalone and SCOUT TIA V4.4 HF2.
The download includes the following components:

  • Delta setup for SIMOTION SCOUT and SCOUT standalone V4.4 HF4
  • TIA Portal client setup for SIMOTION SCOUT TIA V4.4 HF4 (incl. CamTool V3.0 SP3 HF1)

A prerequisite for the installation is that SCOUT, SCOUT standalone or SCOUT TIA of version V4.4 HF2 has already been installed.

The setup of hotfix 4 for SCOUT TIA is a TIA Portal client setup.
The prerequisite is that TIA Portal framework V13 has already been installed on the engineering computer.

Caution
Please note that SIMOTION SCOUT TIA V4.4 HF4 can only be installed with the Totally Integrated Automation Portal V13. Installation with V13 SP1 is not possible, and will only be supported by a future SIMOTION SCOUT TIA V4.4 HF.

Additional information on the V4.4 HF4 is provided in the notification of release for delivery under entry ID 107586910.

Additional downloads:
The following downloads are available to upgrade the SIMOTION firmware from V4.4 HFx to HF4:

  • SIMOTION C kernel/firmware V4.4 HF4 see entry ID 31263919

  • SIMOTION D kernel/firmware V4.4 HF4, see entry ID 31045047

  • SIMOTION Firmware Support Package (FWSP) for the device Update Tool,
    see entry ID 33119786

More detailed information on the SIMOTION V4.4 HF4 can be taken from the release for delivery under entry ID 107586910
 

SCOUT and SCOUT standalone:
The zipped SCOUT V4_4 HF4.zip includes the following components:

  • Delta setup SCOUT V4.4 HF4 (CD_1) for SIMOTION SCOUT and SCOUT standalone V4.4 HF2
  • Readme files
    • Liesmich_SCOUT.rtf
    • Readme_SCOUT.rtf
    • Leggimi_SCOUT.rtf
    • Lisezmoi_SCOUT.rtf

Safety information
Please read item ID 109740097 

A debugged CamTool V3.0 SP3 HF1 can be found under entry ID 108740800.

  SCOUT_V4_4_HF4.zip ( 1007256 KB )

 


SIMOTION SCOUT TIA:
The zipped SIMOTION SCOUT TIA V4_4 HF4.zip includes the following components:

  • TIA Portal client setup for SIMOTION SCOUT TIA V4.4 HF4 (incl. CamTool V3.0 SP1 HF1)
  • Start.exe
  • Start.exe.manifest
  • Subfolder
    • Disk1
    • MigTool
    • ScoutTia
  • Readme files
    • Liesmich.rtf
    • Readme.rtf
    • Leggimi.rtf
    • Lisezmoi.rtf


Safety information
Please read item ID 109740097 


Instructions for the download

The download is divided into several files. Please download all the files into the same directory and execute the file ending with .exe. The files will now be combined and you can execute the setup.

   SIMOTION_SCOUT_TIA_V44_HF4_for_TIAP_V13.exe ( 2657 KB )
   SIMOTION_SCOUT_TIA_V44_HF4_for_TIAP_V13.001 ( 683593 KB )
   SIMOTION_SCOUT_TIA_V44_HF4_for_TIAP_V13.002 ( 683593 KB )
   SIMOTION_SCOUT_TIA_V44_HF4_for_TIAP_V13.003 ( 683593 KB )
   SIMOTION_SCOUT_TIA_V44_HF4_for_TIAP_V13.004 ( 296112 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.