×
Siemens Industry Online Support
Siemens AG
Entry ID: 108165711, Entry date: 08/18/2017
(9)
Rate

PROFINET - An Overview of the Most Important Documents and Links

  • Entry
This page gives you an overview of the most important PROFINET application examples, FAQs and other items in the Industry Online Support. Furthermore, at the end of this page are a number of links to other offerings for PROFINET like brochures, courses and catalog information, for example.




PROFINET Functions


This link list is for the entries concerning the most important PROFINET functions.

Application examples

SIMOTION & SINAMICS: Bumpless Media Redundancy with PROFINET IRT (MRPD)
Application Guideline for Implementing the Switch-Off Concepts With PROFIenergy
PROFIenergy - Saving Energy with SIMATIC S7 (STEP 7 V5.5)
SIMATIC & SIMOTION: Configuring RT communication between SIMATIC and SIMOTION (I-Device)
SIMOTION & SINAMICS: Bumpless Media Redundancy with PROFINET IRT (MRPD)
Diagnostics in User Program with S7-1500
Network and Communication diagnostics
Automatic commissioning of a PROFINET IO system
Integration of an AS-i System into PROFINET with the IE/AS-i LINK PN IO (Configuration 7)
IWLAN: Setup of a Wireless LAN in the Industrial Environment
IWLAN Configuration Using RCoax Cable in a PROFINET IO Environment (Configuration 6)
Configuring standard machines in TIA Portal (configuration control)
Library for PROFINET data records
PROFINET Asset Management

FAQs

SIMOTION: Diagnostic functions for PROFINET and PROFIBUS
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, clock-synchronized mode, system redundancy and option handling?
Which IO controllers and IO devices support the following functions in STEP 7 V5.x: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
FAQ collection for the Development Kit

Manuals

SIMATIC NET Basics of IWLAN
Configuration Examples for S7-400H with PROFINET SIMATIC S7-400H as of V6.0
Basic Functions for Modular Machines
SIMATIC PROFINET PROFINET with STEP 7
SIMATIC STEP 7 Basic/Professional V15.1 and SIMATIC WinCC V15.1

Further Information

PROFINET Overview
Brochure "Enhanced productivity through the fast and open Ethernet standard"
PROFINET Truck

Services

SITRAIN courses for PROFINET

 

Commissioning


This link list is for entries that support you in commissioning a PROFINET IO system.

Application examples

PROFINET IO - Configuration & Diagnostics
PRONETA Basic 3.2 Commissioning and Diagnostics Tool for PROFINET
Creating Documentation Components for PROFINET IO Networks.
Determining the transmission time for typical configurations on Industrial Ethernet

Tools

SIMATIC Automation Tool - the commissioning and service operation tool for SIMATIC modules
PRONETA Basic 3.2 Commissioning and Diagnostics Tool for PROFINET
Primary Setup Tool (PST)
Compatibility Tool for Automation and Drive Technology

Services

SITRAIN courses for PROFINET

Manuals

Documentation for the automation system S7-1500 and the ET 200MP distributed -I/O system
Documentation for the distributed I/O system ET 200
Documentation for the distributed I/O system ET 200SP
Documentation for distributed I/O system ET 200AL

Further Information

PROFINET in Mechanical Engineering - Function Overview


Compatibility & Performance


This linklist includes FAQs about the compatibility and performance of different configurations.

FAQs

Which PROFINET services are supported by SIMATIC panels.
Which controllers can be used to set up a PROFINET field bus in PCS 7?
Which PROFINET devices support media redundancy and which system redundancy?
Which PROFINET functions are supported by SIMOTION and SINAMICS?
Which PROFINET nodes support the extended PROFINET diagnostics and what do you have to configure?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) with topological configuration and device replacement without topological configuration?
Compatibility Tool for Automation and Drive Technology

Performance Information

Determination of the PN response time for typical configurations in the PROFINET IO
Determining the transmission time for typical configurations on Industrial Ethernet

Videos

PROFINET Performance Video


Configuration & Programming Tips


This link list is for tips and tricks for configuring and programming PROFINET plants.

Application examples

Configuration and Application of the PROFINET I-Device Function
Configuring standard machines in TIA Portal (configuration control)
S7-1200 als PN-DP-Gateway
PROFINET in Process Automation with SIMATIC PCS 7
IWLAN: Setup of a Wireless LAN in the Industrial Environment
Isochronous mode with PROFINET - an example with SIMATIC S7-1500
SINAMICS V: Acyclic communication between SIMATIC S7-1500 and SINAMICS V90 via PROFINET
SINAMICS V: Position Control with SIMATIC S7-1200 TO and SINAMICS V90 PN (S mode)
SINAMICS V: Speed Control with SINAMICS V90 and SIMATIC S7-300 via PROFINET
High-performance measurement technology in PROFINET environment

FAQs

In WinCC (TIA Portal), how do you configure a connection between WinCC Runtime Advanced or HMI Panel and an S7 controller over Industrial Ethernet (PROFINET)?
In STEP 7 V12 SP1 (TIA Portal), how do you set the PROFINET update time of an IO device and where do you find an overview of the update times of all the PROFINET nodes?
How do you read out the IP address of the PROFINET interface of a S7-1500 CPU in the user program?
How can you reconfigure the PROFINET interface with the program control instructions of the S7-1200?
How do CPUs of the S7-1200/S7-1500 series react in the case of IO access errors to the input parameters of a block?
How do you configure and parameterize a PROFINET IO device on a SIMATIC S7 with STEP 7 V5?
How do PROFINET IO controllers behave in the case of error when accessing the data of a shared device?
SIMOTION: Where can I find the GSDML file for the PROFINET connection of a SIMOTION control as I-Device?
How do you find out the status of the stations of a DP master system or of a PROFINET IO system?
Why does the CP 1616 / CP 1604 as PROFINET IO controller and/or PROFINET IO device not go into data exchange mode after the configuration has been successfully loaded?
How do you achieve Shared Device with CPU S7-400F and SINAMICS S120 in the TIA Portal with SIMATIC Safety V13 SP1 and higher?
How do you achieve Shared Device with S7-1500 F-CPU and SINAMICS S120 in the TIA Portal with SIMATIC Safety V13 SP1 and higher?
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
SIMOTION, PROFINET: A SIMOTION is also connected to a controller as I-Device in the same project

Further Information

CPU-CPU Communication with SIMATIC Controllers

Industrial Ethernet


This list includes links to helpful entries, tools and services for setting up and analyzing Industrial Ethernet networks.

Application examples

Setup and Configuration of a Redundancy via PRP and HSR
Security with SIMATIC NET

Further Information

Popular topic pages
SIMATIC NET Basics of IWLAN
CPU-CPU Communication with SIMATIC Controllers
Videos on "SINEMA Server"
Industrial Communication, Identification & Locating (Videos)


PROFINET in Process Automation


Learn how PROFINET and SIMATIC PCS 7 interact:

PROFINET in Process Automation with SIMATIC PCS 7


Training


SITRAIN:

SITRAIN – Digital Industry Academy
SITRAIN personal – Germany
Courses for industrial communication
PROFINET


SITRAIN - UK and Ireland
SITRAIN - USA
SITRAIN - Australia
SITRAIN - Canada


Further Information


This list contains links to other websites about PROFINET.

PROFINET Overview
PROFIBUS user organization
PROFINET Certificates
Technical Forum - Conference "Communication / Networks"
Industry Mall: PROFINET Product View
"Minute PROFINET" playlist on YouTube
YouTube channel of the PROFINET user organization
CPU-CPU Communication with SIMATIC Controllers



Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit