×
Siemens Industry Online Support
Siemens AG
Type de contribution : Exemple d’application ID de la contribution : 108416478, Date de la contribution : 12/04/2016
(12)
Évaluer

Safety for Buildings with LOGO! 8 and LOGO! CMR (Set 12)

  • Contribution
  • Concerne le/les produits(s)
The LOGO! 8 and the LOGO! CMR can be used to monitor a building and notify the user locally or via SMS in the event of a risk.

Task
In building management systems, risk prevention and timely alarming play an ever increasing role. With this in mind, the following areas of a building should be monitored with sensors:

  • Basement for unexpected water ingress
  • Duct under basement of building for overflow of the ground-water level
  • Ground floor and basement windows for housebreaking
  • Rooms for housebreaking
  • All building areas for fire

If one of the above mentioned faults or risks occur, the user is to be informed via SMS.

Solution
The figure below shows an overview of the most important components of the solution:



Figure 1


The automation solution uses a LOGO! 8 connected to a LOGO! CMR module to monitor building areas and functions.
If a fault or risk occurs, an SMS is sent to the user and an alarm message is displayed on site on the LOGO! display. In addition, an acoustic alarm device with flashing light is activated in the building.

Advantages
This application example on hand offers you the following advantages:

  • Cost-effective and simple security monitoring of buildings
  • Very user friendly thanks to automatic alarm function via SMS in case of a fault or risk in the building
  • Prevention of water damage to floors and walls in the building
  • Expandable with additional sensors
  • Sends alarm messages in case of wire break or possible sabotage of the wires
  • Planning safety due to a configuration successfully tested
  • Error prevention with tested code and step-by-step instructions

Documentation and Example Project
  Flyer (152,3 KB)
  Documentation (1,8 MB)
Registration required LOGO!Soft Comfort project and configuration file for LOGO! CMR (81.1 KB)




Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Évaluer la contribution
pas d'évaluation
Requêtes et commentaires
Que voulez-vous faire ?
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport