×
Siemens Industry Online Support
Siemens AG
Entry type: Application example, Entry ID: 108740380, Entry date: 10/24/2017
(12)
Rate

Open user communication to 3rd party control system (CLX/GLX controller)

  • Entry
  • Associated product(s)
This library allows to communicate via a standard protocol (TCP/IP) between SIMATIC S7-1200/S7-1500 and Rockwell ControlLogix/GuardLogix without using a Gateway.

To communicate between different controllers of different manufacturers, several options are available. One is the possibility of using a gateway. Another one is the use of own communication blocks for the controllers.

Solution
The libraries in this article provide communication blocks for the communication between S7-1500/S7-1200 controllers and ControlLogix/GuardLogix controllers. They provide a function block for the S7-1500/S7-1200 and an AOI for the ControlLogix/GuardLogix.


Fig. 01

Advantages
This article offers you the following advantages:

  • communication blocks which are flexible to use (as Server or Client, for sending or receiving, ...)
  • easy-to-use and easy-to-adapt program blocks.
  • detailed step-by-step instructions for the use of the libraries

Documentation and Projects
 Documentation (2,0 MB) (2,0 MB) 
 Registrierung notwendig  Library for STEP 7 V13 (766,7 KB) 
 Registrierung notwendig  Library for STEP 7 V14 SP1 (326,3 KB) 
 Registrierung notwendig  Library for Automation Studio 5000 (6,0 KB) 

Last Changes 
Update to STEP V14 SP1

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.