×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 10880206, Entry date: 06/18/2015
(3)
Rate

How do you install the WinCC Smart Tools?

  • Entry
  • Associated product(s)
You can install the WinCC Smart Tools with the user-defined WinCC Setup when installing WinCC.

In order to add or remove software components at a later date, you simply run the WinCC Setup again (in this case the procedure is similar to when you initially install WinCC).

Description

Installation of Smart Tools in WinCC V6.x
 

No. Procedure
1 Run WinCC Setup
Insert the WinCC CD. Usually WinCC Setup starts automatically.
If WinCC Setup doesn't start automatically, start it manually:
  • In the case of an initial installation via "Control Panel > Software > Add New Program".
  • In the case of a retro-installation via "Control Panel > Software > Change or Remove Programs > SIMATIC WinCC Vx.x > Change/Remove".
  • Directly from the WinCC CD.
     

Select "Install SIMATIC WinCC".
 


Fig. 01

2 Run User-defined Setup
  • If reinstalling, you select the button for "User-defined Installation".
  • In the case of a retro-installation, you select the button for installing and uninstalling components.
     


Fig. 02

3 Select Smart Tools
In the "Select Components" dialog you select the "Smart Tools" component from the list on the left.
The available "Smart Tools" are then displayed in the selection window on the right. Now you can select the Smart Tools by checking the relevant option boxes. These Smart Tools are then installed upon completion of Setup.
 


Fig. 03
 

Note
You might have to use the scroll bar to have the "Smart Tools" item displayed.

4 Continue installing
Finish the installation procedure by pressing the "Next" button.

Installation of Smart Tools in WinCC V7.0 
 

No. Procedure
1 Run WinCC Setup
Insert the WinCC DVD. Proceed as follows to start the WinCC Setup manually.
  • In the case of reinstallation, via "Control Panel > Software > Add New Program".
  • In the case of a retro-installation, via "Control Panel > Software > Change or Remove Programs > SIMATIC WinCC Vx.x > Change/Remove".
  • Directly from the WinCC DVD via "DVD drive > InstData > WinCC > setup > Setup.exe
2 Selection for Installation / Uninstallation
Click on the button "Select the components for installation/uninstallation".
   


Fig. 04

3 Select Smart Tools
In the "Select Components" dialog you select the "Smart Tools" component from the list on the left.
The available "Smart Tools" are then displayed in the selection window on the right. Now you can select the Smart Tools by checking the relevant option boxes. These Smart Tools are then installed upon completion of Setup.
   


Fig. 05
 

Note
You might have to use the scroll bar to have the "Smart Tools" item displayed.

4 Continue installing
Finish the installation procedure by pressing the "Next" button.

Installation of Smart Tools in WinCC V7.0 SP1 
 

No. Procedure
1 Run WinCC Setup
Insert the WinCC DVD. Proceed as follows to start the WinCC Setup manually.
  • In the case of reinstallation, via "Control Panel > Software > Add New Program".
  • In the case of a retro-installation, via "Control Panel > Software > Change or Remove Programs > SIMATIC WinCC Vx.x > Change/Remove".
  • Directly from the WinCC DVD via "DVD drive > Setup.exe
2 Select Package Installation / User-defined Installation
Select the option "User-defined Installation" and confirm the selection the "Next" button.
   


Fig. 06

3 Select Tools
In the "WinCC Expert" dialog you can install the desired tools by checking the appropriate check boxes.
   


Fig. 07
 

Note
You might have to use the scroll bar to have the "WinCC Expert" item displayed.

4 Continue installing
Finish the installation procedure by pressing the "Next" button.
5 Select the Smart Tools
You can select the Smart Tools during the WinCC Setup by selecting "Customized" for the scope of installation in the "SIMATIC WinCC Smart Tools Setup".
   


Fig. 08
 

In the Setup window that then opens, you can select the Smart Tools that you wish to install.
 


Fig. 09

Additional Keywords
WinCC Tag Simulator, Communication Configurator, Cross Reference Wizard, WinCC Documentation Viewer, TAG Export/Import, Dynamic Wizard Editor, Add-ons, Additional software

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.