×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 108819464, Entry date: 04/25/2016
(6)
Rate

Announcement of product phase-out for the 1st Generation Basic Panels

  • Entry
  • Associated product(s)
The 1st Generation Basic Panels will be declared phase-out products as per Oct. 1, 2016. This does not concern the two key versions, KP300 Basic mono PN and KP400 Basic color PN.

The 1st Generation SIMATIC HMI Basic Panels have been actively marketed since the beginning of 2009. These products are scheduled to be phased out as per Oct. 1, 2016. The devices will still be available as new parts as usual.

As stipulated in the notice of discontinuation, the spare parts and repair service is scheduled to continue during the next 10 years. More information on the spare parts service is provided under Spare parts and repair service.

Phased-out products are not recommended for new applications. For new machines and systems, we recommend that you use the successor products 2nd Generation Basic Panels. A brief overview about the advantages is provided in the following paragraph respectively under Basic Panels 2nd Generation.

When migrating to the Basic Panels 2nd Generation, lots of benefits result regarding the commissioning, operation and servicing of the operator panels, together with minimum migration expenditure.

During commissioning, you benefit from:

  • User-friendly backup and restore of configuration, operating system and firmware via USB stick with series machines
  • Flexible connection options of, for example, mouse or keyboard via USB

  • Installation compatibility with Comfort Panels

Multiple HMI options result from:

  • The high resolution and extensive range of display colors,
  • the innovative user interface with intuitive usability (e.g. scrolling in lists) as well as
  • new controls and graphics for an attractive machine design

The service can be easily simplified through:

  • The archiving options and thus simplified fault diagnostics
  • the device replacement without PC and engineering software via Backup/Restore using a USB stick
  • the integrated web browser for, e.g., fast access to the web server of the S7-1200 or S7-1500 controllers

The project is easily migrated via a device change in WinCC (TIA Portal). You can, of course, migrate your existing projects from WinCC flexible with little effort to WinCC (TIA Portal) .

Thus, you can quickly migrate your current configuration cost-efficiently to the 2nd Generation Basic Panels. More information on the migration is provided in the Migration Guide Basic Panels

More information on the migration of your system is provided under Migration of systems (visualization)

Recommended successor devices for the 1st Generation Basic Panels

Basic Panels 1st Generation
Basic Panels 2nd Generation

KTP400 Basic mono PN

KTP400 Basic color PN

6AV6647-0AA11-3AX0

6AV6647-0AK11-3AX0

──►

KTP400 Basic6AV2123-2DB03-0AX0

KTP600 Basic mono PN

KTP600 Basic color PN

6AV6647-0AB11-3AX0

6AV6647-0AD11-3AX0

──►

KTP700 Basic6AV2123-2GB03-0AX0
KTP600 Basic color DP6AV6647-0AC11-3AX0

──►

KTP700 Basic DP6AV2123-2GA03-0AX0
KTP1000 Basic color PN6AV6647-0AF11-3AX0──►KTP900 Basic6AV2123-2JB03-0AX0
KTP1200 Basic6AV2123-2MB03-0AX0

KTP1000 Basic color DP

6AV6647-0AE11-3AX0

──►

KTP1200 Basic DP6AV2123-2MA03-0AX0
TP1500 Basic color PN6AV6647-0AG11-3AX0

──►

KTP1200 Basic6AV2123-2MB03-0AX0


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.