×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 108838150, Entry date: 01/20/2015
(0)
Rate

Hotfix 1 (HF1) for SIMOCODE pro PCS 7 Library V7-V8 Migration V8.0 + SP1

  • Entry
  • Associated product(s)
Software Hotfix 1 for SIMOCODE pro PCS 7 Library V7-V8 Migration V8.0 + SP1 is now available for download. With this download, an existing installation of SIMOCODE pro PCS 7 Library V7-V8 Migration V8.0 + SP1 can be updated to V8.0 + SP1 + HF1.

Software requirements for SIMOCODE pro PCS 7 Library V7-V8 Migration V8.0 + SP1 + HF1

  • An already installed version of PCS 7 Library V7-V8 Migration V8.0 + SP1 is required for the installation of Hotfix 1.

  • The library requires as a minimum SIMATIC PCS7 V8.0.

  • The SIMOCODE ES Premium software is necessary to be able to integrate SIMOCODE pro as an S7 slave.
  • The currently released version of F Systems for PCS 7 is required for programming fail-safe functions using a PROFIsafe module for SIMOCODE pro V.

New features and alterations as compared with previous versions

·         When a PROFIBUS connection to "SIMOCODE pro" device has been interrupted and the status of the device has been changed (e.g. from RUN to STOP) during the interruption phase, on reconnection of PROFIBUS to the device, the command that has been sent before (e.g. START) the interruption of connection would be sent for one cycle to the "SIMOCODE pro" device again and will be executed by device (e.g. Motor would start).

This behavior has been fixed in this version of the library. Now the status and commands will be synchronized first before a command will be sent to the device.

·         The newest version of SIMOCODE pro V GSD (V1.5) has been integrated in this version of library.

Steps to be done for updating existing PCS 7 projects

Steps to be followed:

1.Open the CFC.

2.Import an instance of each of the following blocks:

· SMC_DIR

· SMC_REV

· SMC_STAR

· SMC_REVS

· SMC_DAHL

· SMC_REVD

· SMC_CB

· SMC_POS

· SMC_VAL

at the project (and delete the same again if not required) to trigger an update process of all the imported instances in the project

3.   Compile AS: With Changes only.

4.   Download AS program: With Changes only

5.   AS stop necessary: No

6.   Compile OS: No

List of changed blocks:

Number

Name

Block version

Interface change

(= AS Stop necessary)

Code change

Block Import/ Update required

FB2004

SMC_DIR

1.8

No

Yes

Yes

FB2005

SMC_REV

1.8

No

Yes

Yes

FB2006

SMC_STAR

1.5

No

Yes

Yes

FB2007

SMC_REVS

1.5

No

Yes

Yes

FB2008

SMC_DAHL

1.5

No

Yes

Yes

FB2009

SMC_REVD

1.5

No

Yes

Yes

FB2013

SMC_CB

1.5

No

Yes

Yes

FB2011

SMC_POS

1.6

No

Yes

Yes

FB2010

SMC_VAL

1.5

No

Yes

Yes

FB2012

SMC_OVL

1.3

No

No

No

FB2002

SMC_MEAS.

1.6

No

No

No

FB2000

SMC_DIAG.

1.6

No

No

No

FB2003

SMC_STAT

1.3

No

No

No

FB2014

SMC_TIME

1.2

No

No

No

Hint: The generation of module driver for basic integration of Simocode pro (APL channel driver block FbSwtMMS will be used) will not work after the installation of “SIMOCODE pro PCS 7 Library V8 Migration”.  Users wanting to have module driver generation for basic integration have to uninstall “SIMOCODE pro PCS 7 Library V8 Migration”. 

 

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the ReadMe_OSS file.

Special information for resellers

The information and the license terms in the ReadMe_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

  ReadMe_OSS.rtf (155,8 KB)

    SIRIUS_SC_PRO_PCS_7_V8_0_SP1_HF1_MIGRATION.zip (10996 KB) ( 10996 KB )

Note: The software is subject to export restrictions. The download is only available to registered users

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit