×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109344188, Entry date: 07/10/2015
(6)
Rate

SIMATIC B.Data Start Package (video)

  • Entry
  • Associated product(s)
SIMATIC B.Data supports you in the efficient use of energy and in minimizing your energy costs. The SIMATIC B.Data Start Package enables you to get to know this subject very quickly and conveniently.

With SIMATIC B.Data you have decided on one of the most powerful energy management systems worldwide.

In order to help you to gain access to the system, you will find, among others, tutorials on this support page which clearly explain the system installation at the beginning and the handling of the system. Start the videos and follow the instruction.

The SIMATIC B.Data Start Package also includes projects files that are preconfigured in a way to enable you to quickly connect with the different data sources. Also included are examples such as reports, dashboards or charts based on which you can analyze the acquired data straight away.

This is where you get to GettingStarted:
  Technical set of slides (1,8 MB)

Easy guided access with little engineering effort.
Ready energy reports, a dashboard for energy consumption and production figures.

The packet is prepared for one of the following options:

  • Measured values in WinCC archive,

  • Measured values stored in S7-DB,

  • Measured values directly via 7KM PAC Sentron, 3200/4200.

  • Measured values via *.csv File.

 

Media System
Start the Media System here and follow the instruction or download it onto your hard disk:
Link to the Media System
 Registrierung notwendig  Download Media System (1,3 GB)
 
Flyer "SIMATIC B.Data Start Package: Your introduction to energy-efficient production"
Download Flyer

Project files
Load the project files according to the data source (download):
 Registrierung notwendig  SIMATIC WinCC (220,7 KB)
 Registrierung notwendig  SIMATIC S7-300/S7-400 and S7-1200/S7-1500 (1,2 MB)
 Registrierung notwendig  7KM PAC 3200/4200 (221,7 KB)
 Registrierung notwendig  CSV file (271,0 KB)
 

Software-Requirements

Webinars
We offer webinars to introduce the SIMATIC B.Data starter pack. Our experts explain the requirements and the application. You also have the opportunity to ask our experts your specific questions regarding the application.

Would you like to be invited?

If you do, send us your registration with your contact data with the buzzword “Webinar on SIMATIC B.Data starter pack” to the following contact address
energymanagement.industry@siemens.com.

We will then soon invite you to one of the events.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.