×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109439582, Entry date: 02/16/2015
(0)
Rate

What particular points do you need to watch out for when configuring a TeleService connection to the TS Adapter II with STEP 7 Professional V12 or higher (TIA Portal)?

  • Entry
  • Associated product(s)
With the SIMATIC TeleService software as well as with TIA Portal up to and including V11 you can establish a TeleService connection to the TS Adapter II without specifying user name and password, if the adapter still has its default parameters set.

Description
With TIA Portal V12 and higher you must specify at leas the default user name "ADMIN". We recommend assigning a password in addition to avoid abuse.
Alternatively you can also define your own user name. If you enter the user name and password in the telephone book in the TIA Portal, then you do not have any increased typing for establishing the connection.

Security Notes
Siemens offers products and solutions with industrial security functions which support the secure operation of plants, solutions, machines, devices and/or networks. They are important components in a comprehensive industrial security concept. The Siemens products and solutions continue to be developed under this aspect. Siemens recommends that you keep yourself regularly informed about product updates.
For the safe operation of Siemens products and solutions it is necessary to take appropriate security measures (cell protection concept, for example) and to integrate each component in an overall industrial security concept which is state of the art. This should also cover the third-party products used. Additional information about industrial security is available at:
https://www.siemens.com/industrialsecurity.
In order to keep yourself informed about product updates, we recommend subscribing to our product-specific newsletter. Additional information about this is available at
https://support.industry.siemens.com.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit