×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109474271, Entry date: 03/19/2015
(0)
Rate

How do you configure SIMATIC B.Data data acquisition with the Modbus RTU Gateway of the SENTRON PAC 4200?

  • Entry
  • Associated product(s)
You can use a SENTRON PAC4200 as Modbus RTU Gateway to link SETRON PAC3100 measuring devices to SIMATIC B.Data. This enables you to use measuring devices already in your plant with SIMATIC B.Data.

Instructions
A detailed description is given in the PDF file below.
  109474271_BData_RTU_gateway_en.pdf (1,2 MB)

Security Notes
Siemens offers products and solutions with industrial security functions which support the secure operation of plants, solutions, machines, devices and/or networks. They are important components in a comprehensive industrial security concept. The Siemens products and solutions continue to be developed under this aspect. Siemens recommends that you keep yourself regularly informed about product updates.
For the safe operation of Siemens products and solutions it is necessary to take appropriate security measures (cell protection concept, for example) and to integrate each component in an overall industrial security concept which is state of the art. This should also cover the third-party products used. Additional information about Industrial Security is available here:
http://www.siemens.com/industrialsecurity.
In order to keep yourself informed about product updates, we recommend subscribing to our product-specific newsletter. Additional information about this is available at:
http://support.automation.siemens.com.

Additional Keywords
Acquisition wizard, Third-party driver, Communication channel, Acquisition hardware, Device configuration, IP port, Data points, Address, Register, Data type, Module slot, User-defined configuration, Acquisition, Energy data, Energy data management

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.