×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109474538, Entry date: 06/24/2015
(1)
Rate

3SE / 3SF position switches Hysteresis values when used in safety controllers

  • Entry
  • Associated product(s)
This FAQ describe the hysteresis for slow-action and snap-action contacts

 

QUESTION:

Is the hysteresis the same for slow-action and snap-action contacts?
What contact is more suitable for use in safety controllers (signal change or discrepancy times in the F-CPU)?

 

 

ANSWER:

The hysteresis describes the difference between the operating point and reset point in the case of snap-action contacts. This difference results from the different geometric positions of the snap-action mechanism during switching and reset operations.
In the case of slow-action contacts, the operating point and the reset point are always the same because the actuator head actuates the contact mechanism linearly. There is therefore no hysteresis with slow-action contacts.
The operating distances are largely standardized, and thus it is possible to compare competitors within the usual tolerances. Siemens is the only manufacturer able to offer short-stroke contact blocks for the types of construction 50041 and 50047, which enable the switching operation to be implemented significantly earlier.

The following always applies:

Snap-action contact:
- Switching time including contact bounce NC/NO - contacts approx. 2-5 ms (i.e. the contacts switch almost simultaneously within this time)
- Operating point independent of actuating speed
- Operating point independent of contact erosion
- Hysteresis is approximately 30% to 40% of the operating travel

Slow-action contact:
- Switching time dependent on actuating speed
- NC contact always opens first. The NO contact closes only after the non-overlap distance has been overcome (except for make-before-break contacts)
- Operating point dependent on contact erosion/aging
- No hysteresis


Note
A snap-action contact block is by far the better suited contact for contact interrogation by controllers.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.