×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109474575, Entry date: 03/24/2015
(2)
Rate

How do you achieve Shared Device with S7-1500 F-CPU and SINAMICS S120 in the TIA Portal with SIMATIC Safety V13 SP1 and higher?

  • Entry
  • Associated product(s)
With Shared Device different controllers access one IO device and share the (sub) modules of the IO device. With STEP 7 Safety Advanced V13 SP1 and higher access can also be made to a SINAMICS with drive-based safety.

By using a Standard CPU and an F-CPU from S7-1500 and a SINAMICS S120 drive you can run Shared Device with SIMATIC Safety V13 SP1 (see figure below):

 


Fig.


The following document explains the requirements for achieving Shared Device in this constellation with PROFINET.

  F_Shared_Device_1500F_SINAMICS_en.pdf (1,3 MB)