×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109474935, Entry date: 11/29/2019
(6)
Rate

Latest information about Firmware 1.1/1.2 for the SINAMICS DCP and associated SSPs for STARTER

  • Entry
  • Associated product(s)
Information about firmware 1.1/1.2 for the SINAMICS DCP and associated SSPs for STARTER.

Information about firmware 1.3 can be found here 109773826

Firmware

Firmware V1.2 for SINAMICS DCP

 Registrierung notwendig  SINAMICS_DCP_Firmware_V1_2_HF1.zip (17,4 MB)

 Registrierung notwendig  SINAMICS_DCP_Firmware_V1_2_HF2.zip (17,4 MB)

Note: 

  • Procedure of software upgrade for SINAMICS DCP: See chapter 9.1 (Upgrading software releases) in the operating manual.

 

STARTER SSPDescription of the procedure

 Registrierung notwendig  STARTER_SSP_for_SINAMICS_DCP_V1_1.zip (41,9 MB)

 Registrierung notwendig  STARTER_SSP_for_SINAMICS_DCP_V1_2.zip (31,2 MB)

Note:
  • STARTER versions lower than V4.4.0 do not support the DCP

 Registrierung notwendig  SSP_Update_en.pdf (53,2 KB)

 

Restrictions

  Restrictionlist_DCP_V1.2_en.pdf (163,6 KB)

 

 GSD files for integrating the project in SIMATIC

 Registrierung notwendig  GSD_Profibus_DCP_V_1_1.zip (17,4 KB)

 Registrierung notwendig  GSD_Profinet_DCP_V_1_1.zip (28,2 KB)

The GSD files are valid from version 1.1


 Registrierung notwendig  GSD_Profibus_DCP_V_1_2.zip (19,7 KB)

 Registrierung notwendig  GSD_Profinet_DCP_V_1_2.zip (33,8 KB)

The GSD files are valid from version 1.2

 

Lists of faults and warnings

"alarmlist_*.xml" files are not required to properly operate the firmware and related STARTER. They only contain a text extract of the SINAMICS DC MASTER "alarm messages" in "xml" format (this format ensures that the text is displayed correctly independently of worldwide differing fonts and can thus be correctly converted into other formats).
In some cases, this text extract is required by customers who wish to further use it in their applications resp. integrate it in external units. For this reason, we cannot provide any further support for the SINAMICS DC MASTER.

The lists in the zip-file contain 2 components:
 1. alarmlist basic -> general SINAMICS messages
 2. alarmlist oa -> DC-specific messages

 

 Registrierung notwendig  alarmlist_SINAMICS_DCP_V1_2_eng.zip (69,0 KB)

 

 

STARTER (commissioning tool) 


The latest STARTER version (commissioning tool) for SINAMICS can be ordered as DVD under the following order number:  

6SL3072-0AA00-0AG0 

The DVD can be sourced via the PMD with the appropriate reference source (ORG-ID). 


The STARTER-program can also be downloaded under following link as a ZIP-file: 26233208 

 


Resources required, e.g. to back up the parameter assignment and to update the firmware with memory card

 
To update the firmware, you require:

a memory card (MMC) with the following order number: 6RX1800-0AS03

an SD/MMC card reader on your PC or an appropriate external read-write device, e.g. for a USB interface.


Prerequisites for the firmware update:

  • Memory card is available
  • The read device has been installed on the PC
  • A WinZip program has been installed on the computer

 

Please contact the corresponding Technical Support if you have technical questions:

https://support.industry.siemens.com/sc/ww/de/sc/2090

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.