×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109475044, Entry date: 07/22/2021
(48)
Rate

SINAMICS communication blocks DriveLib for reading and writing drive data within TIA Portal Context

  • Entry
  • Associated product(s)
Here you can find the DriveLib for reading and writing data from and to the SINAMICS S/G converter systems within SIMATIC S7-300/400/1200/1500 at TIA Portal. Note: As from Startdrive V16, the DriveLib library is no longer supplied with Startdrive. As from STEP7 V15.1, these blocks are also provided as instructions.

The objective of the standard "Communication blocks for SIMATIC S7-300/400/1200/1500" blocks is the simple implementation of a cyclic or acyclic communication connection between a SIMATIC S7-300/400/1200/1500 controller in TIA Portal and a drive of a SINAMICS S/G converter system. 

Download user documentation
Documentation for the function blocks for S7 1200 / S7 1500  SINAMICS_Bausteine_fuer_TIA_Portal_S7_1200_1500_07_2021_EN.pdf (3,6 MB)
  
 Documentation for the function blocks for S7 300 / S7 400  SINAMICS_Bausteine_fuer_TIA_Portal_S7_300_400_07_2021_EN.pdf (4,3 MB)
 
Download DriveLib as archived user library

 DriveLib V620 for SIMATIC STEP 7 Professional V16 (archived user library)

To act with archived user libraries is decribed at the online help of the TIA Portal at the section "Retrieving global libraries".

 Provision of DriveLib as archived user library for V16.
 DriveLib Version 620 for S7 1200 / S7 1500 Registrierung notwendig  Drive_Lib_V62_S7_1200_1500.zip (1,5 MB)
 SHA-256 checksum: Registrierung notwendig  Drive_Lib_V62_S7_1200_1500_SHA256zip.txt (1 KB)


 DriveLib Version 620 for S7 300 / S7 400 Registrierung notwendig  Drive_Lib_V62_S7_300_400.zip (1,4 MB)
 SHA-256 checksum: Registrierung notwendig  Drive_Lib_V62_S7_300_400_SHA256zip.txt (1 KB)


Download of existing DriveLib libraries
DriveLib V522 for SIMATIC STEP 7 Professional V15.1 (important update of the Version V52)

As a supplement if Startdrive V15.1 Upd 2 (option package) is not installed.

DriveLib Version 522  Registrierung notwendig  109475044_drivelib_TIA15.1_V522.zip (3.4 MB) 
SHA-512 checksum: Registrierung notwendig  drivelib_TIA15.1_V522_sha512zip.txt (1 KB) 
 

DriveLib V511 for SIMATIC STEP 7 Professional V15

As a supplement if Startdrive V15 Upd 4 (option package) is not installed.

DriveLib Version 511 Registrierung notwendig  109475044_drivelib_TIA15_V511.zip (3.3 MB)
SHA-512 checksum:  Registrierung notwendig  drivelib_TIA15_V511_sha512zip.txt (1 KB) 
 

DriveLib V501 for SIMATIC STEP 7 Professional V14 / V14 SP1

As a supplement if Startdrive V14 SP1 Upd 8 (option package) is not installed.

Note:
This download is an update if Startdrive V14 is available.

DriveLib version. Recommendation: Reinstall this download.

DriveLib Version 501 Registrierung notwendig  109475044_drivelib_TIA14_V501.zip (4.4 MB)
SHA-512 checksum:  Registrierung notwendig  drivelib_TIA14_V501_sha512zip.txt (1 KB) 

Note

The current versions of SINAMICS Startdrive can be downloaded at 109760845.

Additional search terms

FB284, FB285, FB286, blocks, SINA_POS, SINA_SPEED, SINA_PARA

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.