×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109475448, Entry date: 07/03/2015
(9)
Rate

Service Pack 1 with separate Update 2 for SIMATIC CFC V8.1

  • Entry
  • Associated product(s)
Service Pack 1 (SP1) and an Update 2 to be installed separately are available for SIMATIC CFC V8.1. The update software for upgrading installed SIMATIC CFC V8.1, V8.1+SP1 or V8.1+SP1 Update 1 to SIMATIC CFC V8.1+SP1 Update 2 is available for download below.

SIMATIC CFC V8.1+SP1 update software

Registrierung notwendig CFC_V81_SP1_Download.zip (137.9 MB)

The update software SIMATIC CFC V8.1+SP1 contains all software components required for the installation of SIMATIC CFC V8.1+SP1. STEP 7 as of V5.4 SP5 (< V10) is a prerequisite for the installation.

Update 2 for SIMATIC CFC V8.1+SP1 update software

Registrierung notwendig Update_2_for_CFC_V81_SP1.zip (55.0 MB)

The Update 2 for SIMATIC CFC V8.1+SP1 update software should be installed in addition to the SIMATIC CFC V8.1+SP1 update software.

Warning:

You should update existing installations of SIMATIC CFC V8.1+SP1 or SIMATIC CFC V8.1+SP1 Update 1 with the Update 2 for SIMATIC CFC V8.1+SP1 without delay.

Scope of application/validity

Service Pack 1 for SIMATIC CFC V8.1 and Update 2 for SIMATIC CFC V8.1+SP1 are relevant for the following products:

  • SIMATIC CFC V8.1, article number 6ES7658-1EX18-0YA5
  • SIMATIC CFC Upgrade V8.0 to V8.1, article number 6ES7658-1EX18-0YE5

When these products are delivered new, Service Pack 1 for SIMATIC CFC V8.1 and Update 2 for SIMATIC CFC V8.1+SP1 are already included in the scope of supply.

Furthermore, SIMATIC CFC V8.1 is an integral part of the SIMATIC PCS 7 engineering software V8.1+SP1. However, Service Pack 1 for SIMATIC CFC V8.1 and Update 2 for SIMATIC CFC V8.1+SP1 are not yet contained in the SIMATIC PCS 7 engineering software V8.1+SP1. Please use the SIMATIC CFC V8.1+SP1 and Update 2 for SIMATIC CFC V8.1+SP1 update software for the upgrade.

Functional extensions/changes:

You can find information on the changes implemented with SP1 and Update 2 in SIMATIC CFC V8.1 in the readme file, which is contained in the ZIP file below "Readme_CFC_V81_SP1_Upd2.zip" (Section "New features and changes as compared to previous versions").

Registrierung notwendig Readme_CFC_V8.1_SP1_Upd2.zip (72.6 KB)

Compatibility:

The compatibility information in the readme file (contained in the attached file "Readme_CFC_V81_SP1_Upd2.zip") applies to SIMATIC CFC V8.1+SP1 and SIMATIC CFC V8.1+SP1 Update 2. Please also be aware that SIMATIC CFC V8.1+SP1 and SIMATIC CFC V8.1+SP1 Update 2 are not compatible with D7-SYS ≤V8.0

Installation

Please only install the installation file corresponding to your language:

  • English, German, French, Italian, Spanish:
    • CFC_V81_SP1_EU
    • CFC_V81_SP1_UPD2_EU
  • Chinese:
    • CFC_V81_SP1_CHS
    • CFC_V81_SP1_UPD2_CHS

Please read the product information in the readme file (contained in the "Readme_CFC_V81_SP1_Upd2.zip" file below) prior to installation.

In addition, if the component "AS-OS Engineering" (WinCC compiler) is used, please note that a CFC of the identical version must be installed.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.