×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109475495, Entry date: 04/16/2015
(0)
Rate

Delivery Release for packaging units of 10 for selected modules of the scalable SIMATIC ET 200SP distributed I/O system

  • Entry
  • Associated product(s)
In addition to the individual packaging of the SIMATIC ET 200SP modules we are now also offering packaging units of 10 for some selected modules.

 

Background
In order to reduce the time required for unpacking the individually packed ET 200SP modules and also to save the disposal costs for the packaging material previously used, we are now also offering packaging units of 10 for some selected SIMATIC ET 200SP modules.

Effective April 04, 2015 the following modules will be available both in packaging units of 1 and in packaging units of 10.

ET 200SP Module

Packaging Unit (VPE)

Article No.

DI 8x24VDC Basic

VPE 1

6ES7 131-6BF00-0AA0

VPE 10

6ES7 131-6BF00-2AA0

DI 8x24VDC Standard

VPE 1

6ES7 131-6BF00-0BA0

VPE 10

6ES7 131-6BF00-2BA0

DI 16x24VDC Standard

VPE 1

6ES7 131-6BH00-0BA0

VPE 10

6ES7 131-6BH00-2BA0

DQ 4x24VDC/2A Standard

VPE 1

6ES7 132-6BD20-0BA0

VPE 10

6ES7 132-6BD20-2BA0

DQ 8x24VDC/0.5A Standard

VPE 1

6ES7 132-6BF00-0BA0

VPE 10

6ES7 132-6BF00-2BA0

DQ 16x24VDC/0.5A Standard

VPE 1

6ES7 132-6BH00-0BA0

VPE 10

6ES7 132-6BH00-2BA0

BaseUnit Type A0

w/o AUX terminals,

load group bridged to the left

VPE 1

6ES7 193-6BP00-0BA0

VPE 10

6ES7 193-6BP00-2BA0

BaseUnit Type A0

with AUX terminals,

load group bridged to the left

VPE 1

6ES7 193-6BP20-0BA0

VPE 10

6ES7 193-6BP20-2BA0

BaseUnit Type A0

w/o AUX terminals,

load group connected to the left

VPE 1

6ES7 193-6BP00-0DA0

VPE 10

6ES7 193-6BP00-2DA0

BaseUnit Type A0

with AUX terminals,

load group connected to the left

VPE 1

6ES7 193-6BP20-0DA0

VPE 10

6ES7 193-6BP20-2DA0

 

Please note the new ordering procedure
When you order modules in
packaging units of 10 please note the new ordering procedure compared to the previous system SIMATIC ET 200S.

·         The packaging units of 10 (VPE 10) of the ET 200SP have their own article number.

·         Always order the number of modules and not the no. of packaging units (VPE)

·         In the case of packaging units of 10 you must always order multiples of 10 pcs.

·         The price for both packaging units is always listed per unit.

Example

You require 20 I/O modules type DI 8x24VDC Basic.

If you want individually packed modules please order 20 x 6ES7 131-6BF00-0AA0

If you want 2 packages with 10 modules each please order 20 x 6ES7 131-6BF00-2AA0

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.