×
Siemens Industry Online Support
Siemens AG
文档类型 产品通知 文档编号 109475509, 文档发布日期 2015年4月22日
(1)
评估

Delivery Release for SIMATIC WinCC/ChangeControl V7.3 and SIMATIC WinCC/Audit V7.3

  • 文档
  • 涉及产品
Effective immediately, SIMATIC WinCC/ChangeControl V7.3 and SIMATIC WinCC/Audit V7.3 are released for delivery. WinCC/ChangeControl V7.3 and WinCC/Audit V7.3 are independent and full version products and will replace the direct predecessor variant. Sale of the predecessor versions ends with the availability of SIMATIC WinCC/ChangeControl V7.3 and SIMATIC WinCC/Audit V7.3 .

1. The new functions of Version 7.3 at a glance

  • SIMATIC WinCC/Audit V7.3 now offers a more intuitive configuration by the integration into the Configuration Studio, as well as a improved user management due to the integration with SIMATIC-Logon.

  • The runtime functionality of Audit has been enhanced with respect to monitoring of the Login/Logout actions.

  • A user-friendly option is now available in the Audit Viewer with which enquiries to the Audit database can be formulated, incl. expanded filter mechanisms.

  • The version check has also been expanded with respect to versioning of the most different WinCC documents, incl. archiving and restoration of WinCC projects, as well as the history display across all projects.

  • Additional support for the following operating system versions:

·  Windows 8.1 Professional 32-Bit / 64-Bit

·  Windows 8.1 Enterprise 32-Bit / 64-Bit

·  Windows Server 2012 R2 Standard / 64-Bit

 

2. Upgrade and Compatibility

    Please note that SIMATIC WinCC/ChangeControl V7.3 and SIMATIC WinCC/Audit V7.3 require SIMATIC WinCC V7.3 as basis. For the use of WinCC/ChangeControl and WinCC/Audit you require SIMATIC Logon. Please note the following restrictions concerning the configurations release for Audit V7.3:

    -   The project opened in WinCC Explorer must be located on a local drive of the PC.

    -   The "Client without own project" is not released for Audit V7.3.

    • SIMATIC WinCC/Audit V7.3 has not been released for virtualization.
    • SIMATIC WinCC/Audit V7.3 has not been released for redundancy.
    • When you upgrade Audit V7.2, both Audit configurations and saved Audit Trails can be migrated to Audit V7.3.

     

    3. Delivery Scope and Ordering Data

    The delivery of WinCC/Audit and WinCC/ChangeControl is comprised of a DVD, a USB stick and a Certificate of License.

    SIMATIC WinCC/Audit RC V7.3 

    Basic package for configuration of the Audit Trail incl. RT

    6AV6371-1DV17-3AX0

    SIMATIC WinCC/Audit RT V7.3

    Generation of Audit Trails in RT

    6AV6371-1DV07-3AX0

    SIMATIC WinCC/ChangeControl V7.3

    for project versioning and document control

    6AV6371-1DV27-3AX0

    SIMATIC WinCC/Audit RT V7.3

    Upgrade V7.x -> V7.3

    6AV6371-1DV07-3BX3

    SIMATIC WinCC/Audit RC V7.3 or WinCC Change Control V7.3

    Upgrade V7.x -> V7.3

    6AV6371-1DV17-3BX3

    SIMATIC WinCC/Audit RT V7.3

    Upgrade V6.2 -> V7.3 

    6AV6371-1DV07-3BX4

    SIMATIC WinCC/Audit RC V7.3 or WinCC Change Control V7.3

    Upgrade V6.2 -> V7.3

    6AV6371-1DV17-3BX4

    Online Versions: (OSD)

      

    SIMATIC WinCC/Audit RC V7.3  DL

    Basic package for configuration of the Audit Trail incl. RT

    6AV6371-1HV17-3AX0

    SIMATIC WinCC/Audit RT V7.3  DL

    Generation of Audit Trails in RT

    6AV6371-1HV07-3AX0

    SIMATIC WinCC/ChangeControl V7.3  DL

    for project versioning and document control

    6AV6371-1HV27-3AX0

    SIMATIC WinCC/Audit RT V7.3 DL

    Upgrade V7.x -> V7.3

    6AV6371-1KV07-3BX3

    SIMATIC WinCC/Audit RC V7.3 DL or
    WinCC Change Control V7.3 DL

    Upgrade V7.x -> V7.3

    6AV6371-1KV17-3BX3

    SIMATIC WinCC/Audit RT V7.3 DL

    Upgrade V6.2 -> V7.3 

    6AV6371-1KV07-3BX4

    SIMATIC WinCC/Audit RC V7.3 DL or
    WinCC Change Control V7.3 DL

    Upgrade V6.2 -> V7.3

    6AV6371-1KV17-3BX4

     

     

     

     

     

     

     

    安全性信息
    为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
    https://www.siemens.com/cybersecurity#Ouraspiration.
    对统计的支持
    用该功能可根据所需数量输出搜索结果的IDs (格式 .txt)

    生成列表
    复制URL
    在新设计中显示此页面
    mySupport Cockpit
    相关链接