×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109475571, Entry date: 11/14/2019
(6)
Rate

SIMATIC/SIMOTION Weihenstephan Standards

  • Entry
  • Associated product(s)
This application supports in integrating the Weihenstephan Standards into SIMATIC controllers and the motion control system SIMOTION. The Weihenstephan Standards (WS) define a universal communication interface for connecting machines to higher level data acquisition systems or MES (Manufacturing Execution systems). They also define the data which must be provided for acquisition.

Task
A machine builder is requested to deliver a Weihenstephan Standards compliant machine into a production line. The integration of the Weihenstephan Standards shall be possible without much engineering, test, etc. effort.

 

 
 

 

Solution
Siemens supports the machine builder in integrating a Weihenstephan Standards compliant solution for SIMATIC controllers and the motion control system SIMOTION.

  • Automatic generation of the corresponding data blocks from the device description file PDACONF.xml
  • Reduced engineering effort by means of predefined and tested library blocks to integrate a compliant Weihenstephan server functionality incl. example call
  • Reduced integration costs through standardized data interfaces
  • Program and State Management according to Weihenstephan for SIMATIC S7-1200/S7-1500 controllers incl. HMI for Comfort Panels
  • High acceptance of the standard in the beverage sector, food production, …

In addition the Weihenstephan client functionality is available for SIMATIC controllers. It can be used, e.g. for machine internal communication to a printer, scanner, …

The software is integrated in the machine application in STEP 7 V5.x by using the ProjectGenerator SIMOTION easyProject for SIMATIC or SIMOTION.

ProjectGenerator: 51339107

PDI (Plant Data Interface) data points: 86302104

Downloads
Note: The software located in this section is based on Weihenstephan Standards Version 08

  STEP 7 Professional / Basic V13 SP2 (TIA Portal)
  For the usage in newer STEP 7 versions see corresponding system manuals (Compatibility of projects/PLC programs)

    SIMATIC S7-1200/S7-1500
        SIMATIC Manual CommunicationProtocol 01/2016 (1,3 MB)
        SIMATIC Manual ProgramStateManagement 02/2017 (1,8 MB)
       Registrierung notwendig  LWeihStd SIMATIC V1.0.6 (1,9 MB)
       Registrierung notwendig  LWeihStd Example SIMATIC V1.0.4 (STEP 7 Professional only) (7,7 MB)
       Registrierung notwendig  WS TIA GenTool V1.0.0 (24,2 KB)

Additional search terms
motioncontrol_apc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Hinweis: Das Feedback bezieht sich immer auf den vorliegenden Beitrag. Ihre Nachricht wird an die Redakteure im Online Support gesendet. In einigen Tagen erhalten Sie von uns eine Antwort, wenn Ihr Feedback das erfordert. Ist für uns alles klar, werden wir Ihnen nicht mehr antworten.