×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109475573, Entry date: 03/28/2017
(1)
Rate

SIMATIC Library LPrintMark - Print Mark Acquisition with TO Measuring Input

  • Entry
  • Associated product(s)
The blocks of the present library support the user in acquiring print marks via the technology object measuring input in the automation system SIMATIC S7-1500 or SIMATIC S7-1500T.



Often in synchronous operations, the phase between the master axis and the slave axis is not the crucial factor. More the phase between the master axis and the product or rather the material that is transported via the slave axis is relevant.

Possible reasons for arising deviations between product and feeding axis are:

  • Slippage between product and axis

  • Wearing of rollers

  • Material faults or rather tolerances of the product

  • Intervention of machine operators

The blocks of the LPrintMark library are dedicated to support the user in acquiring these deviations or rather displacements by means of the technology object (TO) measuring input. The deviation is the calculated difference between an specified (expected) setpoint position and the measured value. The handling of the TO measuring input and the subsequent calculation of the present difference are the main features of the library blocks.

Downloads

STEP 7 Professional V14 (TIA Portal)
For the usage in newer STEP 7 versions see corresponding system manuals (Compatibility of projects/PLC programs)

SIMATIC S7-1500/S7-1500T
  Manual SIMATIC Library LPrintMark 10/2016 (979,4 KB)
 Registrierung notwendig  LPrintMark SIMATIC V1.0.0 (323,8 KB)


Additional Keywords 
motioncontrol_apc_applications, foil feed, feeder, registration mark, eye mark, flow wrapper, tubular bagging machine, Folienabzug, Schlauchbeutel

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit