×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109475708, Entry date: 11/12/2015
(0)
Rate

SIMATIC PCS 7 in the pharmaceutical industry “Blood Plasma Fractionation” (demo project)

  • Entry
  • Associated product(s)
SIMATIC PCS 7 and SIMATIC BATCH are used to illustrate and manage the blood plasma fractionation process with the required high level of efficiency, quality and performance.

Blood plasma fractionation is the process by which proteins are obtained from the human blood plasma. This process involves several phases and takes place under strict guidelines and strictly controlled ambient conditions.

The application example is realized as a SIMATIC PCS 7 multiproject in accordance with ISA-88 and provides a template that comprises all typical components, their open- and closed-loop control, the necessary logic and locking as well as the visualization. It is modularly structured and based on standardized equipment and control modules.

 
The following equipment modules are included:
  • Unit for thawing deep-frozen blood plasma
  • Unit for the production of coagulation factor VIII
  • Production line for blood plasma fractionation by adding ethanol
In the application example, the sequence of the entire process is controlled via SIMATIC BATCH.
 
Advantages
Using the application example has the following advantages:
  • A reduction of the knowledge necessary to develop applications
  • A decrease in the configuration effort
  • More flexible setup and adaptation due to equipment modules

Validity
SIMATIC PCS 7 V8.1
SIMATIC BATCH V8.1

Documentation and Project
  Documentation (1,8 MB)
 Registrierung notwendig  Sample project for PCS 7 V8.1 (238,6 MB)

Further Information
Media system - Pharma Demo Applications
Application example - SIMATIC PCS 7 in the pharmaceutical industry "Fermentation"
Application example - SIMATIC PCS 7 in the pharmaceutical industry “Freeze Dryer”
Application example - PCS 7 Unit Template "CIP - Cleaning in Place"

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
undefined.