×
Siemens Industry Online Support
Siemens AG
Type de contribution : Informations sur le produit ID de la contribution : 109475885, Date de la contribution : 01/12/2017
(3)
Évaluer

Link collection on the topic of SINUMERIK Safety Integrated

  • Contribution
  • Concerne le/les produits(s)
This product news contains a link collection about the topic of "SINUMERIK Safety Integrated" and "SINUMERIK Safety Integrated plus".

Calculation of safety functions

Safety Evaluation Tool

For the Calculation of safety functions, Siemens provides our customers the "Safety Evaluation Tool" (SET). This tool allows to perform safety functions according to EN ISO 13849 and IEC 62061.

Under the following link, you find more information on the Safety Evaluation Tool

Safety Evaluation Tool

SISTEMA

For the calculation of safety functions according to EN ISO 13849, the IFA (Institute for Occupational Health and Safety of the German Social Accident Insurance) provides the software wizard SISTEMA (safety of controllers on machines). This Windows tool supports you when assessing the safety of controllers according to EN ISO 13849.
You can find additional information on the software wizard SISTEMA under the following link.

SISTEMA

PFH values

The current PFH values can be found in our Safety Evaluation Tool.

Further, an additional PFH value document is maintained for SINUMERIK and SINAMICS, which is provided at the following link.

PFH value document

Application examples for the calculation of safety functions for SINUMERIK

SINUMERIK 808

An application example for "Safe Torque Off" including calculation of the safety function according to EN ISO 13849 and IEC 62061 is provided for SINUMERIK 808.

For additional information, please contact your Siemens Personal Contact.

SINUMERIK 828

An application example for safety functions for a machine with 6 axes and 2 spindles is provided for SINUMERIK 828.

For additional information, please contact your Siemens Personal Contact.

SINUMERIK 840D sl

Application examples for the calculation of safety functions are provided for SINUMERIK 840D sl, which you can find at the following link.

Calculation of safety functions for a horizontal axis

Calculation of safety functions for a vertical axis

Mode selection via standard components

Application examples for SINUMERIK 840D sl

Instructions for the acceptance test

Instructions Acceptance test SINUMERIK 840D sl

Example for the acceptance test

Example Acceptance test SINUMERIK 840D sl

Commissioning example

A commissioning example is provided for SINUMERIK 840D sl. You can find this example at the following link:

Commisisoning example

Configuration example

A configuring example for a machine with 3 axes and one spindle is provided for SINUMERIK 840D sl.

For additional information, please contact your Siemens Personal Contact.

Safe communication

Application examples for networking are provided for secure communication with a SINUMERIK 840D sl. You can find these examples at the following links.

Secure linking between two SINUMERIK 840D sl

I-Device linking between a SINUMERIK 840D sl and a SIMATIC IM151-8F CPU

Secure linking between a SINUMERIK 840D sl and a SIMATIC IM 151-7F CPU

Emergency Stop in PL e

This application examples shows how the safety function "Emergency Stop" can be performed in Performance Level e.

Emergency Stop in PL e

SINAMICS brake test

The brake test function in SINAMICS can also be used in combination with SINUMERIK Safety Integrated

SINAMICS brake test

Application example for SINUMERIK 828

SINAMICS brake test

The brake test in SINAMICS can be used for SINUMERIK 828.

Brake test for SINUMERIK 828

Certifications

SINUMERIK 828

A TÜV certificate is provided for SINUMERIK 828, which you can find at the following link.

TÜV Süd

SINUMERIK 840D sl

IFA and TÜV certificates are provided for SINUMERIK 840D sl, which you can find at the following links.

Manufacturer Declaration SINUMERIK 840D sl

IFA (Institute for Occupational Health and Safety of the German Social Accident Insurance)

TÜV Rheinland of North America

TÜV Rheinland

Safety Integrated Function Descriptions

SINUMERIK 828

A Function Description for Safety integrated is provided for SINUMERIK 828, which is provided at the following link.

SINUMERIK 828

Enter the search term "Safety integrated" to find the current description of functions for Safety Integrated.

SINUMERIK 840D sl

A Function Description for Safety integrated is provided for SINUMERIK 840D sl, which is provided at the following link.

SINUMERIK 840D sl

Enter the search term "Safety integrated" to find the current description of functions for Safety Integrated.

SINAMICS

A Function Description for Safety integrated is provided for SINAMICS, which is provided at the following link.

Drive engineering

Enter the search term "Safety integrated" to find the current description of functions for Safety Integrated.

Possilbe encoder connections for SINUMERIK Safety Integrated

You will find information about connecting encoder systems following the link:
Connecting encoder systems 

You will find a list about the encoder systems with Drive CliQ following the link:
Connencting Drive CLiQ systems

Internet presence

General Information on the topic of Safety Integrated at Siemens is provided on our website Functional Safety.

Functional Safety

SINUMERIK Safety Integrated

Additional information on SINUMERIK Safety Integrated is provided on the Internet on the Safety Integrated product pages.

Safety Integrated with SINUMERIK 828

Safety Integrated with SINUMERIK 840D sl

Image film

Two image films for SINUMERIK Safety Integrated are provided. You can find these films at the following links.

SINUMERIK Safety Integrated

SINUMERIK Safety Integrated plus

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport
Pages thématiques concernant cette contribution