×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109476109, Entry date: 12/20/2018
(7)
Rate

What are the system requirements for Online Software Delivery (OSD)?

  • Entry
  • Associated product(s)
In order to be able to download and transfer software and license products provided for downloading in the OSD you should check the following system requirements and make any necessary settings.

Supported Browser Versions
To make optimum use of Online Software Delivery (OSD) we recommend the latest version of one of the following browsers:

  • Internet Explorer
  • Edge
  • Chrome
  • Firefox

Browser Settings
In the browser settings you enable the following settings:

  • "Allow session cookies"
  • "Allow JavaScript"

Further information and help for the settings for each browser is available via the links in the following table:
 

Setting "Allow session cookies" Setting "Allow JavaScript" 
Internet Explorer Help Internet Explorer Help 
Edge Help Edge Help
Chrome Help Chrome Help 
Firefox Help Firefox Help 

We also recommend that you disable the Internet Explorer default setting "Do not save encrypted pages to disk". This setting is to be found in the "Internet Properties" in the "Advanced" tab.
 


Fig. 1 

Requirements for License Transfer
For transferring licenses you need the latest version of the Automation License Manager (ALM) or of the TIA Administrator. The current version and other useful information is available as a download in Entry ID 114358.

Required Settings for the Download of Licenses
If you have problems displaying OSD, check with your System Administrator whether you have access (Proxy/Firewall) to the following domains:

  • mall.industry.siemens.com
  • automation.siemens.com
  • osd-ak.automation.siemens.com

System Requirements Testing
To check that the settings you have made are correct you can transfer a test license via OSD. Proceed as follows for this:

  1. To transfer a test license you must open OSD via one of the license handling programs. For this you start the TIA Administrator and you open OSD via the "Download software" tile. Alternatively you can start the ALM and open OSD via the link "Web License Key Download".
  2. In OSD you go to the "Help" tab and click "System test".
     

    Fig. 2
     
  3. Click the "Transfer license(s)" field and drag-and-drop the license to the desired target drive (in the TIA Administrator you click the "Transfer license(s)" button. A dialog opens for selecting the target directory).
     

    Fig. 3
     
  4. Confirm the message that follows with "Yes".
  5. After successful transfer the test license is on your selected target drive.
     

    Fig. 4
     

Additional Keywords
SWDL, LKDL, SUS, DL

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.