×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109476335, Entry date: 01/30/2019
(4)
Rate

SINAMICS Firmware Version 4.7 SP3 HF2 for SINAMICS products G120 (CU230P-2, CU240B/E-2, CU250S-2), G120C, G120D (CU240D-2, CU250D-2), G110M and SIMATIC ET200pro FC-2

  • Entry
  • Associated product(s)
In this article you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.7 SP3 HF2.

Important Note

The SINAMICS G120 Firmware Version 4.7 SP3 has achieved the milestone "Phase-out announcement" on 01.10.2018. With this background, we recommend using the latest SINAMICS G firmware. The milestone P.M410 "Product Cancellation" for V4.7 SP3 is planned for 01.10.2019.


For the latest firmware version please refer to the article 67364620.


Third-party software - Licensing terms and copyright information 

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the READ_OSS.HTM file.


Special information for resellers 
The information and the license terms in the READ_OSS.HTM file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.


Availability of Source Code
Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.



Siemens AG 

Digital Factory

Customer Services DF&PD

DF CS SD CCC TS

Gleiwitzer Str. 555

90475 Nuernberg, Deutschland

Internet: http://www.siemens.com/automation/support-request

Tel.: +49 911 895 7222


  READ_OSS.HTM (2,1 MB)


Current list of secondary conditions of the SINAMICS G120 for firmware V4.7 SP3

 SINAMICS_G120_V473_Restrictions.pdf (23,8 KB)

 

Function restrictions of the G120 firmware V4.7 SP3 HF2 that have been resolved

 Corrected_functional_restrictions_G120_V4.7_SP3_HF2.pdf (32,9 KB)


Instructions for updating the firmware of the SINAMICS G120

When upgrading, please refer to the instructions, Chapter "Firmware update" in the operating instructions of the particular Control Unit.

For example, you can find the firmware update instructions for CU240B-2 and CU240E-2 here:

 Instructions_Firmwareupdate_G120_CU240BE-2_ENG.pdf (389,6 KB)

Note
:

The zip file on the SD memory card must be unzipped to the root directory.
An SD memory card with at least 256 MB must be used.
Memory cards larger than 2 GB are not supported.
The SD-CARD 512 MB EMPTY can be ordered by specifying the following order number 6SL3054-4AG00-2AA0.


Provision of the SINAMICS G120 multicard V4.7 SP3 HF2

The content of the SINAMICS G120 multicard described above can be downloaded here:

Note:
From version V4.7 HF3, the runtime SINAMICS G120 firmware is not subject to any export restrictions as the output frequency has been limited to 550 Hz.
It is not subject to the Iran embargo, and is not listed in the EC Dual Use regulation. (AL = N).
It does not involve a US product (ECCN = N).

Alternatively, the SINAMICS G120 multicard V4.7 SP3 HF2 (SD card) can be ordered using the following order number
6SL3054-7TB00-2BA0.

 

List of faults and alarms

List of faults and alarms for CU230P-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120P in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, support can no longer be guaranteed for the G120P product.

alarmlist_g120_cu230p_v04705500_chs.xml (380.8 KB)
alarmlist_g120_cu230p_v04705500_eng.xml (411.7 KB)
alarmlist_g120_cu230p_v04705500_esp.xml (433.9 KB)
alarmlist_g120_cu230p_v04705500_fra.xml (444.7 KB)
alarmlist_g120_cu230p_v04705500_ita.xml (439.5 KB)
alarmlist_g120_cu230p_v04706000_deu.xml (417.4 KB)
alarmlist_g120_cu230p_v04705500_rus.xml (551.0 KB)

alarmlist_g120_cu230p_v04705500_jpn.xml (459.3 KB)

 

  

List of faults and alarms for the CU240B-2 and CU240E-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the G120 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G120 product.

alarmlist_g120_cu240b_e_v04705500_chs.xml (621.1 KB)
alarmlist_g120_cu240b_e_v04705500_eng.xml (671.6 KB)
alarmlist_g120_cu240b_e_v04705500_esp.xml (707.1 KB)
alarmlist_g120_cu240b_e_v04705500_fra.xml (726.7 KB)
alarmlist_g120_cu240b_e_v04705500_ita.xml (712.8 KB)
alarmlist_g120_cu240b_e_v04706000_deu.xml (680.8 KB)
alarmlist_g120_cu240b_e_v04705500_rus.xml (899.0 KB)

alarmlist_g120_cu240b_e_v04705500_jpn.xml (748.7 KB)

 

List of faults and alarms for the CU240D-2 and CU250D-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120D in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G120D product.

alarmlist_g120d_v04705500_chs.xml (709.5 KB)
alarmlist_g120d_v04705500_eng.xml (768.5 KB)
alarmlist_g120d_v04705500_esp.xml (807.3 KB)
alarmlist_g120d_v04705500_fra.xml (829.4 KB)
alarmlist_g120d_v04705500_ita.xml (814.9 KB)
alarmlist_g120d_v04706000_deu.xml (775.5 KB)
alarmlist_g120d_v04705500_rus.xml (1.0 MB)

alarmlist_g120d_v04705500_jpn.xml (858.2 KB)

 

List of faults and alarms for CU250S-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G120 product.

alarmlist_g120_cu250s_v04705500_chs.xml (1.1 MB)
alarmlist_g120_cu250s_v04705500_eng.xml (1.2 MB)
alarmlist_g120_cu250s_v04705500_esp.xml (1.2 MB)
alarmlist_g120_cu250s_v04705500_fra.xml (1.3 MB)
alarmlist_g120_cu250s_v04705500_ita.xml (1.3 MB)
alarmlist_g120_cu250s_v04706000_deu.xml (1.2 MB)
alarmlist_g120_cu250s_v04705500_rus.xml (1.6 MB)

alarmlist_g120_cu250s_v04705500_jpn.xml (1.3 MB)

 

List of faults and alarms of the G120C

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120C in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G120C product.

alarmlist_g120c_v04705500_chs.xml (422.0 KB)
alarmlist_g120c_v04705500_eng.xml (459.5 KB)
alarmlist_g120c_v04705500_esp.xml (485.2 KB)
alarmlist_g120c_v04705500_fra.xml (498.7 KB)
alarmlist_g120c_v04705500_ita.xml (489.5 KB)
alarmlist_g120c_v04706000_deu.xml (465.3 KB)
alarmlist_g120c_v04705500_rus.xml (621.0 KB)

alarmlist_g120c_v04705500_jpn.xml (516.3 KB)

 

List of faults and alarms of the G110M

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the G110M in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G110M product.

alarmlist_G110M_v04705500_chs.xml (533.3 KB)
alarmlist_G110M_v04705500_eng.xml (577.4 KB)
alarmlist_G110M_v04705500_esp.xml (609.4 KB)
alarmlist_G110M_v04705500_fra.xml (626.0 KB)
alarmlist_G110M_v04705500_ita.xml (615.0 KB)
alarmlist_G110M_v04706000_deu.xml (585.2 KB)
alarmlist_G110M_v04705500_rus.xml (776.2 KB)

alarmlist_G110M_v04705500_jpn.xml (646.0 KB)

 

List of faults and alarms of the ET200pro FC-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the ET200pro FC-2 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the ET200pro FC-2 product.

alarmlist_et200pro_v04705500_chs.xml (552.8 KB)
alarmlist_et200pro_v04705500_eng.xml (600.7 KB)
alarmlist_et200pro_v04705500_esp.xml (633.8 KB)
alarmlist_et200pro_v04705500_fra.xml (651.3 KB)
alarmlist_et200pro_v04705500_ita.xml (640.0 KB)
alarmlist_et200pro_v04706000_deu.xml (609.0 KB)
alarmlist_et200pro_v04705500_rus.xml (813.2 KB)

alarmlist_et200pro_v04705500_jpn.xml (671.9 KB)

 

GSD files for project integration into the PROFIBUS configuring tool

PROFIBUS GSD files can be downloaded in the following entries:

 

GSDML files for integrating projects into the PROFINET configuring tool

PROFINET GSDML files can be downloaded in the following entries:


EDS files for integrating projects into the CANopen configuring tool

The EDS files for integrating projects into the CANopen configuring tools can be downloaded from the following entry: (see 48351511)

 

STARTER

Within the scope of firmware version V4.7 SP3, the new STARTER V4.4 SP1 is made available (see product information109475420 and is available as download under 26233208).


As an alternative to installing STARTER V4.4 SP1, with the installation of the available SINAMICS Support Packages (SSP) for firmware V4.7 SP3 (see 109476629) existing STARTER installations can be supplemented. The required STARTER version is specified in the appropriate SSP readme file.

With the SSP, new functions can be configured in the V4.7 SP3 firmware using STARTER.

Within the scope of revising and simplifying the commissioning wizards, SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" have been introduced.

 

For "Standard Drive Control", after the commissioning wizards have been completed and when the drive is switched on for the first time, a shortened motor data identification routine is carried out, and then the drive is immediately ramped-up to the setpoint (p1900 = 12). This setting cannot be changed.

 

For "Dynamic Drive Control", as default setting, a shortened motor data identification routine is selected after the drive is switched on for the first time and then it ramps-up to the setpoint (p1900 = 12). The motor data identification routine can be configured. A rotating measurement is recommended to achieve a higher accuracy and dynamic performance of the closed-loop control. For the motor data identification routine, you can select during commissioning whether the drive shall run up directly to the setpoint or whether another Power ON command is required.

 

Under "Expert", you will find the traditional wizard providing a multitude of setting options.
With this setting, you can configure the motor data identification routine. For the motor data identification routine, while commissioning you can select whether the drive should immediately ramp-up to the setpoint, or a new switch-on command is required.

 

 

Warning

 

 

When selecting motor data identification (motor ID) with subsequent ramp-up to the setpoint speed (p1900 = 11 or 12; 12=standard setting with "Standard Drive Control" and "Dynamic Drive Control"), the motor is, upon the first Power ON command, directly accelerated to the setpoint speed, following a short delay time caused by the motor ID (approx. 8 to 30 s). For additional information, see 109480663.

 

In order to be able to use the revised commissioning wizards for G120 Control Units with PM240, PM240-2 and PM330, as well as for G120C, it is absolutely necessary to upgrade STARTER to version V4.4 SP1.

  

Startdrive

Within the scope of firmware version V4.7 SP3, for Startdrive V13 SP1 (see 107657741) Support Package V4.7 SP3 is available (see 109477753).

When importing the Support Packages in an existing Startdrive V13 SP1 installation, new functions in firmware V4.7 SP3 can be used with Startdrive. Included here is the revised commissioning wizard, which can be used with SINAMICS G120 Control Units in conjunction with PM240, PM240-2, PM330 Power Modules and with G120C.

 

Within the scope of revising and simplifying the commissioning wizards, SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" have been introduced.

 

For "Standard Drive Control", after the commissioning wizards have been completed and when the drive is switched on for the first time, a shortened motor data identification routine is carried out, and then the drive is immediately ramped-up to the setpoint (p1900 = 12). This setting cannot be changed.

 

For "Dynamic Drive Control", as default setting, a shortened motor data identification routine is selected after the drive is switched on for the first time and then it ramps-up to the setpoint (p1900 = 12). The motor data identification routine can be configured. A rotating measurement is recommended to achieve a higher accuracy and dynamic performance of the closed-loop control. For the motor data identification routine, you can select during commissioning whether the drive shall run up directly to the setpoint or whether another Power ON command is required.

 

Under "Expert", you will find the traditional wizard providing a multitude of setting options.
With this setting, you can configure the motor data identification routine. For the motor data identification routine, while commissioning you can select whether the drive should immediately ramp-up to the setpoint, or a new switch-on command is required.

 

Warning

 

 

When selecting motor data identification (motor ID) with subsequent ramp-up to the setpoint speed (p1900 = 11 or 12; 12=standard setting with "Standard Drive Control" and "Dynamic Drive Control"), the motor is, upon the first Power ON command, directly accelerated to the setpoint speed, following a short delay time caused by the motor ID (approx. 8 to 30 s). For additional information, see 109480663.

 

It is not necessary to install a new Startdrive version.

  

 

IOP/BOP-2

With firmware version V4.7 SP3, the commissioning wizard has been revised and the IOP has been supplemented to include extended manual operation. The revised commissioning wizard, which can be used with SINAMICS G120 Control Units in conjunction with PM240, PM240-2, PM330 Power Modules and with G120C.

 

Within the scope of revising and simplifying the commissioning wizards, SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" have been introduced.

 

For "Standard Drive Control", after the commissioning wizards have been completed and when the drive is switched on for the first time, a shortened motor data identification routine is carried out, and then the drive is immediately ramped-up to the setpoint (p1900 = 12). This setting cannot be changed.

 

For "Dynamic Drive Control", as default setting, a shortened motor data identification routine is selected after the drive is switched on for the first time and then it ramps-up to the setpoint (p1900 = 12). The motor data identification routine can be configured. A rotating measurement is recommended to achieve a higher accuracy and dynamic performance of the closed-loop control. For the motor data identification routine, you can select during commissioning whether the drive shall run up directly to the setpoint or whether another Power ON command is required.

 

Under "Expert", you will find the traditional wizard providing a multitude of setting options.
With this setting, you can configure the motor data identification routine. For the motor data identification routine, while commissioning you can select whether the drive should immediately ramp-up to the setpoint, or a new switch-on command is required.

 

 

Warning


 

When selecting motor data identification (motor ID) with subsequent ramp-up to the setpoint speed (p1900 = 11 or 12; 12=standard setting with "Standard Drive Control" and "Dynamic Drive Control"), the motor is, upon the first Power ON command, directly accelerated to the setpoint speed, following a short delay time caused by the motor ID (approx. 8 to 30 s). For additional information, see 109480663.

 

Expanded functionality is supported with the new IOP version from V1.6 and higher. A complete overview of the expanded functionality for IOP V1.6 can be taken from the sales and delivery release109476464. In order to upgrade an existing IOP the entry ID also includes an IOP firmware download.

The BOP-2 operator panel (Order No.: 6SL3255-0AA00-4CA1) is automatically updated when using firmware V4.7 SP3.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.