×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109476571, Entry date: 10/26/2018
(15)
Rate

Operating system update: CPU410-5H Process Automation

  • Entry
  • Associated product(s)
Firmware download PCS 7 CPU 410-5H

Current firmware version for SIMATICPCS 7 CPU 410-5H Process Automation:

  • 6ES7410-5HX08-0AB0

Instructions

for the operating system update of CPU 410-5H Process Automation, see entry: 85196540.

Please note
The update is subject to export restrictions. Only registered users have the option of downloading the update file. Due to the numerous requests, the registration process for export-restricted downloads can take several days.

Note
The CPU 410-5H firmware V8.2.0 can be used independently of SIMATIC PCS 7 V9.0. This also allows you to benefit from the corrections for the CPU410-5H and the new behavior of the load memory using SIMATIC PCS 7 V8.x.


Downloads

Download firmware version V8.0 (backup only – June 2013)

Start of delivery of the CPU 410-5H

Note that the transfer of the V8.0 firmware is only possible when the CPU is in STOP mode.

MLFBDownload
CPU 410-5H Process Automation6ES7410-5HX08-0AB0Download unterliegt ExportcontrolleRegistrierung notwendig 4105HX08_V800.exe (5.7 MB)




    

Download firmware version V8.0.1 (backup only – Nov. 2013)

Corrections in CPU 410-5H firmware V8.0.1

  • Correction of the feedback signals (BUSY and RETVAL) of SFC 51 with the SSL 0c3C with synchronous processing.
  • Sending messages through the CPU also works without restriction after locking and releasing messages in combination with acknowledgment (Alarm8/Alarm8P) (internal ref. no 570182/329941).
  • Correction of fault 4550 090c 3c03 (intern ref. no. 736394).

Firmware update in RUN:
Within a faul-tolerant system firmware update in RUN is possible, from firmware version V8.0.0 to version V8.0.1.

MLFBDownload
CPU 410-5H Process Automation6ES7410-5HX08-0AB0Download unterliegt ExportcontrolleRegistrierung notwendig CPU4105HX08_V801.zip (6.1 MB)





Download firmware version V8.0.2 (backup only – May 2014)

Corrections in CPU 410-5H firmware V8.0.2

  • After a temporary interruption of the lower sync cable, for example, due to pulling and plugging, sometimes the sync coupling could no longer be established on this cable (internal ref. no. 738697).
  • Depending on the load, loading large F-blocks in redundant mode triggered the hardware sign-of-life monitoring of the CPU (internal ref. no. 985705/984854).
  • A monitoring time set too high for H-communication connections could trigger a CPU fault (internal ref. no. 969654).

Firmware update in RUN:
Within a redundant system firmware update in RUN is possible, from firmware version V8.0.1 to version V8.0.2.
Note that upgrading from V8.0.0 to V8.0.2 is only possible when the CPU is in STOP mode.

MLFBDownload
CPU 410-5H Process Automation6ES7410-5HX08-0AB0Download unterliegt ExportcontrolleRegistrierung notwendig CPU4105HX08_V802.zip (5.6 MB)Download unterliegt ExportcontrolleRegistrierung notwendig (6.1 MB)


Download V8.1


Download firmware version V8.1 (backup only – Oct. 2014)

Note that upgrading the CPU 410-5H firmware to V8.1.0 is only possible when the CPU is in STOP mode.

The following behavior is corrected with CPU 410-5H firmware V8.1.0:

  • After a temporary interruption of the lower sync cable, for example, due to pulling and plugging, sometimes the sync coupling could no longer be established on this cable and the MAINT LED is illuminated.
  • After supplementing or deleting a station or module via CiR and then performing a power off/on, the CPU is no longer able to start up in RUN.
  • Fault with identifier W#16#4550/0C10, caused by simultaneous access to multiple field devices with SIMATIC PDM
  • Fault with identifier W#16#4520/8123, for details see Current entry 90039870
  • Fault with identifier W#16#4550/0C0B with monitoring time set very high (> 510s) for H-communication connections

Functional extensions through CPU 410-5H firmware V8.1.0

  • Two PROFINET interfaces of the CPU can be used (as of SIMATIC PCS 7 V8.1)
  • CPU 410 Expansion Packs for increased performance without hardware replacement (as of SIMATIC PCS 7 V8.1)
  • Support of block type changes in runtime (TCiR; as of SIMATIC PCS 7 V8.1)
  • Improved performance when using an integrated PN interface for coupling SIMATIC PCS 7 operator stations

Note that upgrading from V8.0.x to V8.1.0 is only possible in STOP mode of the CPU.
The CPU 410-5H firmware V8.1.0 can be used independent of SIMATICPCS 7 V8.1. You also benefit from the corrections for the CPU410-5H when using SIMATIC PCS 7 V8.0.

MLFBV8.1.0 SHA-256 checksum
CPU 410-5H Process Automation6ES7410-5HX08-0AB0Download unterliegt ExportcontrolleRegistrierung notwendig 4105HX08_V810.exe (6.1 MB)  Registrierung notwendig  4105HX08_V810_hash.txt (1 KB) 





Download firmware version V8.1.1 (backup only – April 2015)

Version 8.1.1 contains the following improved functionality:

  • System availability has been increased by expansion of the correction mechanisms in case of temporary internal inconsistencies. In redundant systems, an automatic resynchronization may thus be started in some rare cases.
  • Optimized handling of synchronization errors between the two CPUs of a redundant system also increases system availability.
  • By expanding the diagnostic functionality in connection with additional PROFIBUS CPs, the switchover time can be further reduced in some cases.
  • Avoidance of a synchronization error in conjunction with calling TCON (FB65) and TDISCON (FB66) blocks in very rapid succession. The blocks are used to establish and terminate connections for open IE communication.
  • The time status at the PN interfaces is now properly applied.

Recommendation: The update to this firmware version should be performed as soon as possible.
CPU 410-5H firmware V8.1.1 can be used independent of SIMATICPCS 7 V8.1. You also benefit from the corrections for the CPU410-5H when using SIMATIC PCS 7 V8.0.

Firmware update in RUN:
Within a faul-tolerant system firmware update in RUN is possible, from firmware version V8.1.0 to version V8.1.1.
Note that upgrading from V8.0.x to V8.1.1 is only possible when the CPU is in STOP mode.

NOTE: When using a PROFINET interface in conjunction with time synchronization over this interface (slave to PNIO), the firmware update in RUN sometimes cannot be performed due to an incorrect configuration. Such an incorrect configuration is characterized by the different settings of CPU0 and CPU1 on the PROFINET interface. In this case, correct the configuration or contact our Customer Support for further assistance.

Product information: PI-A5E32282837-AE_DO.pdf (134.0 KB)
OSS license conditions: OSS_A5E03854325-05.pdf (240.7 KB)

MLFBV8.1.1SHA-256 checksum 
CPU 410-5H Process Automation6ES7410-5HX08-0AB0Download unterliegt ExportcontrolleRegistrierung notwendig 4105HX08_V811.exe (6.1 MB)  Registrierung notwendig  4105HX08_V811_hash.txt (1 KB) 

 

 

Download firmware version V8.1.2 (backup only – Dec 2015)

Version 8.1.2 contains the following improvements:

  • The fault (16#4520D2xx) in conjunction with a program startup time of more than 5 minutes was corrected. Such a long program startup time can occur with a correspondingly long running startup OB (OB100, OB102) or with startup time monitoring > 5 minutes (default: 65s) in conjunction with a missing device or DP slave (internal ref.: 1082167).
  • When an output module was pulled in a PROFINET device, for this module address it was possible that an access ok in the process image was incorrectly generated immediately after an access error in the process image (incoming), (internal ref.: 1389304).

  • When reading the device status on a PROFINET subsystem (0x694 and 0x794 system status list) with SFC51 "RDSYSST", the device status sometimes was not displayed correctly if subslots without user data (e.g. a SCALANCE switch) were configured in the PROFINET device (internal ref.: 1336667).

  • When a previously configured and loaded network at the PROFINET IO interface X8 is deleted, LED BUS8F was incorrectly activated (internal ref .: 1327528).

  • When the available memory was no longer sufficient during an interface change of a function block in runtime (TCIR), in rare cases the system went into DEFECT mode and the entire automation system stopped (internal ref.: 1502467).

  • In an H-system with a higher-level time synchronization, in very rare cases the time of the automation system was set incorrectly for one update cycle immediately after coupling and updating (internal ref.: 1492108).

  • In extremely rare cases, the CPU could go into DEFECT mode with the error message "Checksum error" (ID: 16#4533) and the additional information 16#EDA4 (internal ref.: 1442082).

  • The highly sporadic fault in the automation system with the identifier: 16#4520 D26x was corrected (internal ref.: 1296418).

Version 8.1.2 also contains the following correction:

  • The SNMP data of the CPU410 have been harmonized with the other SIMATIC CPUs. This changes the content of the SNMP variables "ifDescr" and "sysLocation".These changes especially improve the interaction with the SINEMA servers (internal ref.: 1401960 and 1401964).

Recommendation: The update to this firmware version should be performed as soon as possible.

Firmware update in RUN:
Within a faul-tolerant system firmware update from firmware version V8.1.1 to version V8.1.2 is possible in RUN.

Product information: PI-A5E33040434-AE_DO.pdf (40.8 KB)
OSS license conditions: OSS_A5E03854325-05.pdf (240.7 KB)

MLFBV8.1.2 SHA-256 checksum
CPU 410-5H Process Automation6ES7410-5HX08-0AB0Download unterliegt ExportcontrolleRegistrierung notwendig 4105HX08_V812.exe (6.1 MB)  Registrierung notwendig  4105HX08_V812_hash.txt (1 KB) 

 

 

Download firmware version V8.1.3 (backup only – April 2017)

The following corrections were made in firmware version V8.1.3:

  • A synchronization error in connection with reading the system status list
  • (SSL) 16#694 by means of SFC51 and Req=0 has been corrected (internal ref.: 1631973).
  • In very rare cases, the CPU could change to the Defective operating state in the event of configuration changes in Run on a single CPU (non-redundant operation). (Internal ref.: 1566295)
  • Optimization of memory compression in connection with PBK instances (PCS 7 messages). (Internal ref.: 1505052)
  • In the context of HMI read access, the full configuration scope of 39 ANY pointers can now be used. (Internal ref.: 1637821)

In addition, the following functional expansion was implemented:

  • Improvements and expansions relating to service data (internal ref.: 1548865)

Firmware update in RUN:
Within a faul-tolerant system firmware update from firmware version V8.1.2 to version V8.1.3 is possible in RUN.

Product information:  Registrierung notwendig  PI-A5E32282837-AH_DO.pdf (136,4 KB)
OSS license conditions: OSS_A5E03854325-05.pdf (240.7 KB)

MLFBV8.1.3 SHA-256 checksum
CPU 410-5H Process Automation6ES7410-5HX08-0AB0 Download unterliegt Exportcontrolle  4105HX08_V813.exe (6,1 MB)   Registrierung notwendig  4105HX08_V813_hash.txt (1 KB) 

  

Download V8.2


Download firmware version V8.2.0 (backup only – May 2017)

Note that upgrading the CPU 410-5H firmware to V8.2.0 is only possible when the CPU is in STOP mode.

Important information regarding change of CPU behavior caused by firmware V8.2.0
Firmware V8.2 changes the behavior of the CPU load memory. This change is independent of the hardware version.
As of firmware V8.2, the content of the load memory is stored in a non-volatile memory area of the CPU. This means the downloaded program and the configuration do not depend on buffering by a battery. The load memory can only be completely deleted with a memory reset or a factory reset.
Please note:
The CPU signals any existing program by flashing the RUN and STOP LEDs at a different frequency (RUN: 0.5 Hz; STOP: 2 Hz) after the CPU has been switched on. Startup of the CPU can be canceled in case of recommissioning, and a factory reset (see Manual) can be performed before the current program is run.


Functional extensions through CPU 410-5H firmware V8.2.0

PROFINET extensions:

  • Support of redundant PROFINET configurations (R1). The CPU 410 Expansion Pack (PN RED) is required to use this configuration. The procedure for transferring licenses of this Expansion Pack is the same as the procedure for extending the PO volume of the CPU 410.
  • Support of configuration changes during operation of the CPU in the H system (H-CiR) and stand-alone operation (CiR)

  • Support of time synchronization according to the PTCP method and Sequence of Event (SoE)

Security extensions:

  • New protection function for PROFIBUS and PROFINET interfaces (Field Interface Security)

  • Support of SysLog in combination with SIEM systems

Other extensions:

  • The load memory is preserved regardless of buffering by back-up batteries. The CPU can restart independently even without back-up batteries after power failures.

  • The maximum size of data packets for communication was extended from 480 to 960 bytes.

  • In stand-alone operation (Single AS), individual DP stations or PN devices can now be activated or deactivated on PROFBUS and PROFINET by means of the system function D_ACT_DP (SFC 12). This function is not available in case of a redundant configuration.

Additional details on the respective functional extensions is available in the CPU 410 manual.


The following behavior is corrected with CPU 410-5H firmware V8.2.0:

  • The unwanted behavior when using SFC49 "LGC_GADR" to the diagnostic address of the PROFINET IO (see Entry ID: 109736598) has been eliminated.

  • If a PROFINET network was configured to which no PN devices are connected, a switch to the active IO controller of this empty network in the H system could result in a transition of the CPU to the DEFECT operating state and thus in a failure of the entire H system (see Entry ID: 109745029). (internal ref.: 2232241)

  • The behavior during monitoring of a block with multiple instances (multiple devices or multiple windows) has been improved. The automation system now no longer changes to the DEFECT operating state in very rare cases when exiting monitoring (internal ref.: 1926461)

  • During failure of an external DP master (CP443-5DX), the CPU no longer switches to STOP operating state due to an I/O bus error. The CPU 410 tries to initiate a system restart in this case.

  • During monitoring of blocks with conditional jump instructions in the monitoring section, a DEFECT of the CPU could occur in case of specific command combinations. (internal ref.: 1925468)

  • In case of faulty parameter assignment of an area pointer, the system could change to the DEFECT operating state in case of a subsequent write access. (internal ref.: 2091308)

  • When using a fail-safe program for more than 9 years (without switching off the power supply), the CPU could change to the DEFECT operating state. (internal ref.: 2215726)

  • When loading fail-safe blocks, a memory reset request could be issued by the CPU in very rare cases. (internal ref.: 2173858)


    The following changes are the result of correcting the behavior:

    • UDP broadcast telegrams can be no longer received. The type of telegrams is not used in SIMATIC PCS 7.

    • In case of jump instructions the actual data are no longer displayed when monitoring blocks. Actual data are still displayed for all other types of commands.


    CPU 410-5H firmware V8.2.0 can be used independent of SIMATIC PCS 7 V9.0. This means you also benefit from the corrections for the CPU410-5H and the new behavior of the load memory when using SIMATIC PCS 7 V8.x.

    Note that upgrading from V8.0.x or V8.1.x to V8.2.0 is only possible when the CPU is in STOP mode. Make sure that both CPUs of an H system have the same firmware version prior to commissioning.

    Product information:  Registrierung notwendig  PI-A5E32282837-AH.pdf (148,3 KB)
    OSS license conditions:  Registrierung notwendig  PI-OSS_A5E41916916-AA.pdf (339,5 KB)

    MLFBDownload SHA-256 checksum
    CPU 410-5H Process Automation6ES7410-5HX08-0AB0 Download unterliegt Exportcontrolle  4105HX08_V820.exe (6,4 MB)
      Registrierung notwendig  4105HX08_V820_hash.txt (1 KB) 

    Release of CPU 410E

     MLFB Download SHA-256 checksum 
     CPU 410E Process Automation    6ES7410-5HM08-0AB0 Download unterliegt Exportcontrolle  4105HM08_V820.exe (6,4 MB)   Registrierung notwendig  4105HM08_V820_hash.txt (1 KB) 


    Important information 05/2019:

    Please note, that the firmware >=V8.2.0 contains additional improvements in TCiR. Based on this PCS 7 system upgrades to V9.0.x including upgrades of the basis library V9.0.x will be supported in the best way.

     

    Download V8.2.1


    Download Firmware Version V8.2.1 (currend version –  October 2018)

    Important information regarding change of CPU behavior caused by firmware V8.2.0:
    Firmware V8.2 changes the behavior of the CPU load memory. This change is independent of the hardware version. As of firmware V8.2, the content of the load memory is stored in a non-volatile memory area of the CPU. This means the downloaded program and the configuration do not depend on buffering by a battery. The load memory can only be completely deleted with a memory reset or a factory reset.
    Please note:
    The CPU signals any existing program by flashing the RUN and STOP LEDs at a different frequency (RUN: 0.5 Hz; STOP: 2 Hz) after the CPU has been switched on. Startup of the CPU can be canceled in case of recommissioning, and a factory reset (see Manual) can be performed before the current program is run.

    The following behavior is corrected with CPU 410-5H and CPU 410E firmware V8.2.1:

    • The behavior when monitoring blocks has been improved. A change into Defect operating state with identifier 4550 8F01 no longer occurs (Internal ref.: 2573914).
    • In extremely rare cases, the CPU switched to Defect operating state with identifier 4550/8128 when using consistent user data (KND) > 32 bytes as well as switched I/O, with simultaneous loss of synchronization (internal ref.: 2572371)
    • Using PDM and writing a data set by controller application at the same time and on the same periphery station may result in a system shut down in very rare cases (internal ref.: 2587574)
    • Increased robustness for non-standard-compliant messages / message sequences of PROFINET devices (internal ref.: 2369969)
    • In extremely rare cases, a loss of synchronization was possible for OUC connections that had, in principle, been set up but not established and which are, however, actively terminated, in conjunction with time synchronization in SIMATIC mode (time slave) (internal ref.: 2369640).
    • Robustness increase belongs to SNMP protocol failures were done. Additionally, it is now possible to deactivate the SNMP protocol, see Entry-ID: 109760539  (internal ref.: 2377055)
    • After downloading a faulty configuration and subsequently correcting it, the MAINT LED no longer remains constantly lit (internal ref.: 2344532).
    • It could happen sporadically after overall reset and reloading of the controller application that the time of the CPU was no longer synchronized, if one of the CPU internal interfaces was configured as NTP client and another interface as master of the SIMATIC time synchronization. (internal ref.: 2388497).
    • Only for firmware version V8.2: In a configuration without time synchronization of the CPU, the given correction factor of the time by the module properties was not applied. Now again the time correction works correctly (internal ref.: 2533618).
    • When using NTP time synchronization with several NTP servers, the synchronization could fail in rare cases, if the stratum of the NTP servers changes frequently (internal ref.: 2712587).

    The CPU 410-5H firmware V8.2.1 can be used independently of SIMATIC PCS 7 V9.0. This also allows you to benefit from the corrections for the CPU410-5H and the new behavior of the load memory using SIMATIC PCS 7 V8.x.

    Firmware update in RUN:
    Within fault-tolerant systems firmware update is possible in RUN when updating from firmware version V8.2.0 to version V8.2.1.

    Note that upgrading from V8.0.x or V8.1.x to V8.2.1 is only possible when the CPU is in STOP mode. Make sure that both CPUs of an H system have the same firmware version prior to commissioning.

    Product information:  Registrierung notwendig  PI-A5E32282837-AJ_DO.pdf (52,0 KB)
    OSS license conditions:  Registrierung notwendig  A5E41916916-AC.pdf (241,8 KB)

     MLFB V8.2.1 SHA-256 checksum
    CPU 410-5H Process Automation6ES7410-5HX08-0AB0  Download unterliegt Exportcontrolle  4105HX08_V821_.exe (6,4 MB)   Registrierung notwendig  4105HX08_V821_hash.txt (1KB) 
    CPU 410E Process Automation6ES7410-5HM08-0AB0  Download unterliegt Exportcontrolle  4105HM08_V821.exe (6,4 MB)   Registrierung notwendig  4105HM08_V821_hash.txt (1KB) 


    Important information 05/2019:

    Please note, that the firmware >=V8.2.0 contains additional improvements in TCiR. Based on this PCS 7 system upgrades to V9.0.x including upgrades of the basis library V9.0.x will be supported in the best way. 


    For further information on SHA-256 checksum see Entry: 109483101 







    Security information
    In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit