×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109476649, Entry date: 05/12/2015
(17)
Rate

SINAMICS V-ASSISTANT Commissioning tool V1.01.00.18

  • Entry
  • Associated product(s)
The latest version of SINAMICS V-ASSISTANT commissioning tool V1.01.00.18 for the device SINAMICS V90 is provided here:

Description

Supported V90 firmware version: the V-ASSISTANT V1.01.00.18 supports all the official released firmware versions V1.03, V1.03.01, V1.04.00

Please be note: If the V90 firmware version is V1.04.00. (Check the V90 Firmware Version via parameter r29018), need to update the V-ASSISTANT to version V1.01.00.18.

The download file is named as “Sinamics V-Assistant V10100.18.zip". It comprises "Setup.exe" and "Checksum1.0 Value of setup.exe.txt "

  Sinamics_V-Assistant_V1010018.zip (139,5 MB)

Use of SINAMICS V-ASSISTANT is free of charge and does not require a license key to be entered.

Supported languages

The following languages are supported with this version:

English/Chinese/German/French/Italian/Spanish/Portuguese/Turkish

Changes/extension

Following new functions are supported by V-ASSISTANT if V90 firmware V1.04.00 is used:

  • Function of forcing the EMGS signal to logical "1"
  • Function of One-button auto tuning function
  • Optimized some user interfaces e.g. auto tuning
  • "Optimize drive" function can be used in compound control modes in this version
  • German/French/Italian/Spanish/Portuguese/Turkish are supported from this version

How to install SINAMICS V-ASSISTANT

  1. Download the attached ZIP file
  2. Unpack the ZIP file into a target directory on your hard disk.
  3. Start the installation program by double-clicking the “Setup.exe” file.
  4. Finish the installation according to the instructions on the screen
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.