×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109476671, Entry date: 05/07/2015
(0)
Rate

Software SIMOCODE pro PCS 7 Library V8.1 + HF2

  • Entry
  • Associated product(s)
The software SIMOCODE pro PCS 7 Library V8.1 + HF2 is now available for download. With this download, an existing installation of SIMOCODE pro PCS 7 Library V8.1 can be updated to V8.1 + HF2.

Software requirements for SIMOCODE pro PCS 7 Library V8.1 + HF2

  • An already installed version of SIMOCODE pro PCS 7 Library V8.1 is required for the installation.
  • The library requires as a minimum SIMATIC PCS 7 V8.1 and Advanced Process Library (APL).
  • The SIMOCODE ES Premium software is necessary to be able to integrate SIMOCODE pro as a S7 slave.

 

Overview of new features and corrections for PCS 7 SIMOCODE pro Library V8.1 + HF2

  • An update from PCS 7 SIMOCODE pro V8.1 to PCS 7 SIMOCODE pro V8.1 + HF2 does not require a stop of the AS.

 

Corrections:

If SIMOCODE pro V PN device will be configured on an external Profinet interface (e.g.: behind CP 443-1) and not on the internal PLC Profinet interface then Module Fault output (ModF_Act) will be set at MMDiag block on a Warm Restart of the PLC and this means for the system that there is an error in device though device itself is fine.

This issue has been resolved and SIMOCODE pro V PN devices can be configured now on an external Profinet interface.

 

Steps to be done for upgrading existing PCS 7 projects:

  1. Import an instance of MMDiag block at the PCS 7 project to update all instances of the blocks.
  2. Compile and download the AS program with 'Changes only' no PLC restart is necessary.
  3. Set the value of parameter ‘Acc_Id’ at all instances of MMDiag block to ‘1’ if this bug fix applies to your system configuration (SIMOCODE pro V PN devices are configured on an external Profinet interface).

 

List of changed blocks:

 

Number

Name

Block-Version

Interface change (AS stop necessary)

Block Import / Update required

FB1300

MMDiag

2.1

No

Yes

 

Installation notes:

SIMOCODE pro PCS 7 Library V8.1 + HF2 is offered in the form of the download file
“SMCPro_PCS7_V8.0.2.2_V8.1.0.2.zip“. Please exit all STEP 7 applications prior to starting the installation. After having unpacked the *.zip file, please start the program "Start.exe". Please also observe the installation and application notes available in the file \SMCPro_PCS7_V8.1.0.2\DATA1\Readme\MMReadme.rtf.

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the ReadMe_OSS_V8.0.2.2 und ReadMe_OSS_V8.1.0.2 file.

Special information for resellers

The information and the license terms in the ReadMe_OSS_V8.0.2.2 und ReadMe_OSS_V8.1.0.2 file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

  ReadMe_OSS_V8.0.2.2.rtf (83,1 KB)
  ReadMe_OSS_V8.1.0.2.rtf (83,2 KB)

Download

 Download unterliegt Exportcontrolle  SMCPro_PCS7_V8.0.2.2_V8.1.0.2.zip (68,9 MB)
Note: The software is subject to export restrictions. The download is only available to registered users

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.