×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109476672, Entry date: 05/18/2015
(1)
Rate

Hardware Support Package “HSP0115 SIMOCODE pro V Modbus RTU”

  • Entry
  • Associated product(s)
The Hardware Support Package “HSP0115 SIMOCODE pro V Modbus RTU“ for SIMOCODE ES V13 SP1 and STEP 7 V13 SP1 is available for download.

Installing the HSP0115, the hardware catalog of SIMOCODE ES V13 or STEP 7 V13 SP1 can be updated with the
SIMOCODE pro V PN basic unit firmware version V1.2.

In addition, the hardware catalog of SIMOCODE ES V13 can be updated with the SIMOCODE pro V Modbus RTU basic unit.

The HSP is required for parameterization of the SIMOCODE pro basic units as follows:

  • SIMOCODE pro V MR (Modbus RTU)               3UF7012-1AB00-0 and 3UF7012-1AU00-0
  • SIMOCODE pro V PN, FW V1.2                        3UF7011-1AB00-0 and 3UF7011-1AU00-0

  • SIMOCODE pro  V Operator Panel with Display (EN, CN, RU)               3UF7210-1BA00-0

Requirement

The “HSP0115 SIMOCODE pro V Modbus RTU” requires the following installation:

  • SIMOCODE ES V13 SP1 (109347377) or
  • STEP 7 V13 SP1

  • The "HSP_V13SP1_0115_001_SIMOCODE_Modbus_RTU_1.0.isp13"  file must be available on the configuration PC.

Installing HSP in the TIA Portal

  1. Open the TIA Portal with administrator rights.
  2. Select "Tools > Support Packages" from the menu. The "Detail information > Installation of Support Packages" dialog box opens.
  3. Click the "Add from file system" button.
  4. Select the directory of the "HSP_V13SP1_0115_001_SIMOCODE_Modbus_RTU_1.0.isp13" file in the file system.
  5. Click "Open". The file is added in the TIA Portal.
  6. Activate the "

    HSP0115 SIMOCODE pro V Modbus RTU" in the "Detail information" dialog.

  7. Click the "Install" button. A dialog box opens.

  8. Close the TIA Portal.

  9. Click "Next". Installation starts.

Result

After successful installation, the "Detail information" dialog shows the "HSP0115 SIMOCODE pro V Modbus RTU" as installed.

Download

 Registrierung notwendig  HSP_V13SP1_0115_001_SIMOCODE_Modbus_RTU_1.0.isp13.zip (20,8 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.