×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109476692, Entry date: 05/19/2015
(0)
Rate

Product phase-out: EC31 controller (2nd Generation)

  • Entry
  • Associated product(s)
Effective October 1, 2015, the EC31 controller is going to be listed entirely as product phase-out. This means the 2nd Generation of the controller with 4GB Flash Disc user memory is also being phased out.

Effective October 1, 2015, the EC31 controller is going to be listed entirely as product phase-out. This means the 2nd Generation of the controller with 4GB Flash Disc user memory is also being phased out. For new projects, we recommend either realizing the projects with WinAC RTX on Microbox D or switching directly to our new product generation ET 200SP Open Controller with S7-1500 Software Controller and TIA Portal.

Beginning with the start of the phase-out, new parts will most likely still be available for orders until discontinuation. Discontinuation will not become effective before October 2018. After new parts can no longer be ordered, defective devices may be shipped in for identified repair until the end of September 2020. With this type of repair, the original software images (corresponds to version and scope during original delivery) can be installed on the devices when the original packing slip is included.

We recommend that existing customers back up the software installations with an image backup. Information on the backup is described in the manual (entry ID: 37971572) section 9.1.

 

Phase-out affects the following article numbers:

 

Name

Description

Article number

EC31

Core Duo 1.2 GHz processor, 1 GB RAM, 4 GB Flash Disc,
Operating system: WES 2009

SDK

6ES7677-1DD10-0BA0

 

(also corresponds to the article number of the spare part)

EC31-RTX

Core Duo 1.2 GHz processor, 1 GB RAM, 4 GB Flash Disc,
Operating system: WES 2009,
WinAC RTX 2010

6ES7677-1DD10-0BB0

EC31-RTX F

Core Duo 1.2 GHz processor, 1 GB RAM, 4 GB Flash Disc,
Operating system: WES 2009,
WinAC RTX F 2010

6ES7677-1FD10-0FB0

EC31-HMI/RTX

128 PT

Core Duo 1.2 GHz processor, 1 GB RAM, 4 GB Flash Disc,
Operating system: WES 2009,
WinAC RTX 2010,

WinCC flexible 2008 SP2 RT with 128 PT

6ES7677-1DD10-0BF0

EC31-HMI/RTX

512 PT

Core Duo 1.2 GHz processor, 1 GB RAM, 4 GB Flash Disc,
Operating system: WES 2009,
WinAC RTX 2010,

WinCC flexible 2008 SP2 RT with 512 PT

6ES7677-1DD10-0BG0

EC31-HMI/RTX

2048 PT

Core Duo 1.2 GHz processor, 1 GB RAM, 4 GB Flash Disc,
Operating system: WES 2009,
WinAC RTX 2010,

WinCC flexible 2008 SP2 RT with 2048 PT

6ES7677-1DD10-0BH0

EM PCI‑104

Expansion module PCI-104 for EC31

6ES7677-1DD40-1AA0

EM PC

Expansion module PC for EC31

6ES7677-1DD50-2AA0

 

 

 

 

 

 

 

 

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.