×
Siemens Industry Online Support
Siemens AG
寄稿のタイプ: ダウンロード 寄稿のID: 109476710, 寄稿の日付: 06/18/2021
(2)
評価する

Firmware update for SIMATIC ET 200AL CM 4xIO-LINK 4xM12

  • 寄稿
  • 製品に関係する
Firmware update for SIMATIC ET 200AL CM 4xIO-LINK 4xM12 - Latest change: new firmware version V1.2.0 - note removed

Desciption:

When firmware is updated, it must always be updated to the latest version available for the relevant article number. The previous versions of the firmware are only intended as a backup to enable you to downgrade to the original version.
The latest version of firmware in each case is valid for all revision levels of this article number.

A detailed description of performing the firmware update is provided in the entry 109475743.

Overview of article numbers and current firmware versions of the ET 200AL CM 4xIO-LINK 4xM12:

Article number

Software
version

Upgrade by means of...

6ES7147-5JD00-0BA0

 V1.2.0

Recommended for upgrade:
For a  description, see below Update V1.2.0


For STEP 7 as of version 5.5
 Registrierung notwendig  Classic_6ES7147-5JD00-0BA0_V120.ZIP (117,7 KB)(SHA-256)
(Informationen zu SHA-256)


For STEP 7 TIA Portal
 Registrierung notwendig  TIA_6ES7147-5JD00-0BA0_V120.ZIP (117,5 KB)(SHA-256)
(Informationen zu SHA-256)

 V1.1.1

Backup only:
For a  description, see below Update V1.1.1


For STEP 7 as of version 5.5
 Registrierung notwendig  Classic_6ES7147-5JD00-0BA0_V111.ZIP (117,1 KB)
SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  Classic_6ES7147-5JD00-0BA0_V111.txt (1 KB) 


For STEP 7 TIA Portal
 Registrierung notwendig  TIA_6ES7147-5JD00-0BA0_V111.ZIP (116,9 KB)
SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  TIA_6ES7147-5JD00-0BA0_V111.txt (1 KB)

 V1.1.0

Backup only:
For a  description, see below Update V1.1.0


For STEP 7 as of version 5.5
 Registrierung notwendig  Classic_6ES7147-5JD00-0BA0_V110.ZIP (116,5 KB) 
SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  Classic_6ES7147-5JD00-0BA0_V110.txt (1 KB)


For STEP 7 TIA Portal
 Registrierung notwendig  TIA_6ES7147-5JD00-0BA0_V110.ZIP (116,2 KB)
SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  TIA_6ES7147-5JD00-0BA0_V110.txt (1 KB)

 V1.0.3

Backup only:
For a description, see below Update V1.0.3

For STEP 7 as of version 5.5
 Registrierung notwendig  Classic_6ES7147-5JD00-0BA0_V103.ZIP (101,2 KB)

For STEP 7 TIA Portal
 Registrierung notwendig  TIA_6ES7147-5JD00-0BA0_V103.ZIP (101,1 KB) 

 V1.0.2

Backup only:
For a description, see below Update V1.0.2

For STEP 7 as of version 5.5
 Registrierung notwendig  Classic_6ES7147-5JD00-0BA0_V102.ZIP (101,0 KB)

For STEP 7 TIA Portal
 Registrierung notwendig  TIA_6ES7147-5JD00-0BA0_V102.ZIP (101,0 KB)

V1.0.1

Backup only:
For a description, see below Update V1.0.1

For STEP 7 as of version 5.5
Registrierung notwendig Classic_6ES7147-5JD00-0BA0_V101.EXE (219.0 KB)

For STEP 7 TIA Portal
Registrierung notwendig TIA_6ES7147-5JD00-0BA0_V101.EXE (219.0 KB)

V1.0.0

Backup only:

For STEP 7 as of version 5.5
Registrierung notwendig Classic_6ES71475JD000BA0_V100.EXE (219.0 KB)

For STEP 7 TIA Portal
Registrierung notwendig TIA_6ES71475JD000BA0_V100.EXE (219.0 KB)


 Update V1.2.0

The firmware contains the following optimizations:

  • Extension of the usable data width of the IO-Link master to 132 bytes - this means that 4 IO-Link devices with data widths of up to 32 bytes each can now also be used without restriction.

The firmware update is available free of charge for download and can be transferred to the module using standard resources.

The system can be upgraded for a fee at the factory.



Update V1.1.1

The firmware V1.1.1 contains the following optimizations:

  • Improvement of the IO-Link communication during startup with COM3 devices
  • Improvement of the data backup of IO-Link devices with more than 69 parameters
  • Support for the FW update for IO-Link devices


Update V1.1.0

The firmware contains the following changes:

  • Extension of the IO-Link configuration without S7-PCT and the "Master Backup" function
  • Stability improvements in combination with S7-PCT 

  • Improvement of the behavior shown by the PROFINET user data companion when powering up and down the module as well as when re-establishing the ET connection after an interruption. This firmware version should be used when operating the ET 200AL on a third-party (non-SIEMENS) CPU.


Update V1.0.3

The firmware V1.0.3 contains the following optimization:

  • Improvement of the IO-Link communications stability during some IO-Link devices.

 

Update V1.0.2

Adaption to newly specified design instruction of the IO-Link standard and thus improved startup behavior in connection with certain IO-Link devices.

 

 Update V1.0.1

The firmware contains the following optimizations:

  • Support of the user data configuration 4 byte input/4 byte output
  • Improved diagnostic behavior when the fieldbus is interrupted


セキュリティ情報
技術的なインフラストラクチャー、システム、機械とネットワークをサイバー脅威から守るために、現在の技術の状態に応じた全体的なITセキュリティーコンセプトを実装すること(そして持続的に維持すること)が必要です。シーメンスの製品とソリューションはそのようなコンセプトの1つの要素だけを形成します。サイバーセキュリティーについての詳細は以下をご覧ください:
https://www.siemens.com/cybersecurity#Ouraspiration.
寄稿を評価する
評価なし
リクエストとフィードバック
何をしたいですか?
注: フィードバックは常に現在のエントリ / 製品に関連しています。メッセージは、オンラインサポートで作業しているテクニカルエディタに転送されます。フィードバックに応答が必要な場合は、数日以内に返信いたします。これ以上問題がない場合、ご連絡はいたしません。
統計に対するサポート
この機能によって、希望する数に基づく検索結果のIDが出力されます (format .txt)

Generate list
URL をコピーする
このページを新しいデザインで表示する
mySupport コックピット