×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109476797, Entry date: 06/08/2015
(0)
Rate

Why does the CP5622 disappear from the component configurator after restoring the IPC system from a bundle image?

  • Entry
  • Associated product(s)

Description
If you are using a communications processor of the type CP5622 in your SIMATIC IPC, it might happen that the CP disappears from the component configurator after a restart of the IPC. This behavior occurs after the system partition of the IPC system has been restored from a bundle image.

Cause
One possible cause for this behavior is the firmware version of the communications processor. If the version is less than V1.03.08.046, the described behavior occurs.

Remedy
This problem can be remedied by updating the firmware of the communication processor to version V1.03.08.046. The required firmware data and instructions for carrying out the update are available in Entry ID 92275417.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit