×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109476914, Entry date: 04/27/2017
(33)
Rate

What are the differences between the Basic (BA), Standard (ST), High Feature (HF) and High Speed (HS) modules of the ET 200SP and ET 200MP?

  • Entry
  • Associated product(s)
This entry provides you with information about the function classes of the interface modules and IO modules of the distributed IO systems ET 200SP and ET 200MP.

The interface modules and the IO modules of the ET 200MP and ET 200SP are available in the following function classes.

  • Basic (BA): The Basic module is designed for basic requirements.
  • Standard (ST): The Standard module is designed for standard requirements and is used by most customers.
  • High Feature (HF): The High Feature module includes advanced functions.
  • High Speed (HS):The High Speed module is optimized for high speed processing.

Properties of the function classes of the interface modules of the ET 200MP

  109476914_PropertiesFuctionClasses_IM_ET200MP_en.pdf (5,1 KB)

Properties of the function classes of the IO modules of the ET 200MP

  109476914_PropertiesFuctionClasses_IO_ET200MP_en.pdf (94,0 KB)

Properties of the function classes of the interface modules of ET 200SP

  109476914_PropertiesFuctionClasses_IM_ET200SP_en.pdf (6,6 KB)

Properties of the function classes of the IO modules of the ET 200SP

  109476914_PropertiesFuctionClasses_IO_ET200SP_en.pdf (4,3 KB)

Note

  • All ET 200SP IO modules can be used on all ET 200SP interface modules.
  • Exception:
    • PROFIsafe modules cannot be used on a Basic interface module.
    • The technology module TM Timer DIDQ 10x24V cannot be used on the DP interface module.
  • You should note that function restrictions of the interface modules might restrict the IO module functions. For example:
    HF and HS IO modules support the clock-synchronized mode. The Basic, Standard and DP interface modules do no support the clock-synchronized mode.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.